Clock Manager#
Introduction#
The Clock Manager module is responsible for configuring the clock tree in the Si91x system. It enhances the clock management features provided by the GSDK's emlib and device_init services, offering additional functionality for selecting clock sources and setting dividers. This module ensures optimized performance and power efficiency across various system components by managing clock configurations according to application requirements.
Configuration#
The Clock Manager supports a variety of configurations:
Clock Source Selection: Allows specific clock sources to be chosen for different branches.
Divider Configuration: Modifies clock frequencies by setting divider values.
Configuration is typically performed during device initialization using configuration files and source code.
Usage#
The following steps outline typical usage of the Clock Manager:
Initialize the Clock Manager with desired configuration settings.
Set up oscillator sources and configure clock dividers.
Use runtime APIs to manage dynamic clock changes.
Maintain stable clock configurations to ensure system reliability.
Benefits#
Manages complex clock trees efficiently.
Enhances system stability and performance.
Supports a wide range of Si91x devices.
Optimizes power consumption through efficient clock management.
Typedefs#
Typedef to select the clock source for the M4 core in the Si91x SOC.
Functions#
Initializes the M4_SOC and other required clocks.
To configure the M4 core clock source and configure the PLL frequency if selected as source.
To set the selected PLL (Phase-Locked Loop) clock to the desired frequency.
To read the currently active M4 core clock source and its frequency.
Gets the selected PLL (Phase-Locked Loop) clock to the desired frequency.
Controls the selected PLL (Phase-Locked Loop) clock.
Delays execution for the specified number of milliseconds.
Set M4 ULP Processor clock division factor.
Macros#
PLL reference clock frequency value of XTAL CLK.
Max PLL frequency is 180MHz.
Typedef Documentation#
sl_si91x_m4_soc_clk_src_sel_t#
sl_si91x_m4_soc_clk_src_sel_t
Typedef to select the clock source for the M4 core in the Si91x SOC.
This typedef maps to the M4_SOC_CLK_SRC_SEL_T type, which defines the possible clock source selections for the M4 core. The clock source selection impacts the operating frequency and performance characteristics of the M4 processor within the Si91x SOC.
Users can configure the clock source to optimize power consumption or performance based on application requirements.
Note
Ensure that the selected clock source is properly configured and stable before switching to avoid system instability.
Function Documentation#
sl_si91x_clock_manager_init#
sl_status_t sl_si91x_clock_manager_init (void )
Initializes the M4_SOC and other required clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
Corresponding error code on failure.
For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_clock_manager_m4_set_core_clk#
sl_status_t sl_si91x_clock_manager_m4_set_core_clk (M4_SOC_CLK_SRC_SEL_T clk_source, uint32_t pll_freq)
To configure the M4 core clock source and configure the PLL frequency if selected as source.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| M4_SOC_CLK_SRC_SEL_T | [in] | clk_source | Enum value representing different core clock sources. |
| uint32_t | [in] | pll_freq | Desired M4 core frequency in MHz. |
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
Corresponding error code on failure.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_clock_manager_set_pll_freq#
sl_status_t sl_si91x_clock_manager_set_pll_freq (PLL_TYPE_T pll_type, uint32_t pll_freq, uint32_t pll_ref_clk)
To set the selected PLL (Phase-Locked Loop) clock to the desired frequency.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PLL_TYPE_T | [in] | pll_type | Enum specifying the type of PLL to configure. |
| uint32_t | [in] | pll_freq | Desired frequency for the PLL clock (in MHz). |
| uint32_t | [in] | pll_ref_clk | Reference clock frequency for the PLL configuration. |
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
Corresponding error code on failure.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_clock_manager_m4_get_core_clk_src_freq#
sl_si91x_m4_soc_clk_src_sel_t sl_si91x_clock_manager_m4_get_core_clk_src_freq (uint32_t * m4_core_clk_freq)
To read the currently active M4 core clock source and its frequency.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [out] | m4_core_clk_freq | Pointer to a variable where the current core clock frequency will be stored (in MHz). |
Returns
sl_si91x_m4_soc_clk_src_sel_t The currently active core clock source:
0: M4_ULPREFCLK
2: M4_SOCPLLCLK
3: M4_MODEMPLLCLK1
4: M4_INTFPLLCLK
5: M4_SLEEPCLK
sl_si91x_clock_manager_get_pll_freq#
uint32_t sl_si91x_clock_manager_get_pll_freq (PLL_TYPE_T pll_type)
Gets the selected PLL (Phase-Locked Loop) clock to the desired frequency.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PLL_TYPE_T | [in] | pll_type | Enum specifying the type of PLL to configure. |
Returns
uint32_t PLL frequency value in MHz.
sl_si91x_clock_manager_control_pll#
sl_status_t sl_si91x_clock_manager_control_pll (PLL_TYPE_T pll_type, bool enable)
Controls the selected PLL (Phase-Locked Loop) clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PLL_TYPE_T | [in] | pll_type | Enum specifying the type of PLL to control. |
| bool | [in] | enable | Boolean value to enable (true) or disable (false) the PLL. |
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
Corresponding error code on failure.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_delay_ms#
void sl_si91x_delay_ms (uint32_t milli_seconds)
Delays execution for the specified number of milliseconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | milli_seconds | Delay time in milliseconds. |
Note
This function provides a blocking delay.The delay is calibrated based on the SystemCoreClock frequency. If SystemCoreClock < CLOCK_THRESHOLD, the delay is calibrated with a division factor of LOW_FREQ_CLK_DIV_FAC. If SystemCoreClock >= CLOCK_THRESHOLD, the delay is calibrated with a division factor of HIGH_FREQ_CLK_DIV_FAC. This function uses
__NOP()instructions for the delay loop.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_clock_manager_ulp_processor_clk_division#
sl_si91x_clock_manager_ulp_processor_clk_division (uint8_t clk_div)
Set M4 ULP Processor clock division factor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | clk_div | Division factor (the clock will be divided by 2*clk_div) |
This API sets the M4 ULP Processor clock division factor by configuring the clock control register. The division factor is calculated as 2*clk_div, where clk_div is the input parameter.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK - Success.
SL_STATUS_INVALID_PARAMETER - Invalid argument.
Note
This API should be invoked only when the system is in PS2 state, as the source clock in this mode is configured to use a 20 MHz RC.
For more information on status codes, see SL STATUS DOCUMENTATION.