Client#

Note

  • To manage the Wi-Fi interface lifecycle correctly, it's important to use functions like sl_wifi_init(), sl_wifi_connect(), sl_wifi_disconnect(), and sl_wifi_deinit() as intended. Improper sequencing or combining sl_wifi_* and sl_net_* API functions without following the recommended order may lead to unpredictable or undefined behavior.

Functions#

sl_status_t
sl_wifi_connect(sl_wifi_interface_t interface, const sl_wifi_client_configuration_t *access_point, uint32_t timeout_ms)

Connect to the given Wi-Fi AP.

sl_status_t
sl_wifi_disconnect(sl_wifi_interface_t interface)

Disconnect the Wi-Fi client interface.

sl_status_t
sl_wifi_get_signal_strength(sl_wifi_interface_t interface, int32_t *rssi)

Retrieve the RSSI value of the Access Point to which the Wi-Fi client is connected.

sl_status_t
sl_wifi_get_ip_config_failure_reason(sl_status_t *ipv4_status, sl_status_t *ipv6_status)

Get the per-family IP configuration status captured during the last IP configuration.

sl_status_t
sl_wifi_get_sta_tsf(sl_wifi_interface_t interface, sl_wifi_tsf64_t *tsf)

Get the station Timing Synchronization Function (TSF) time which is synchronised with connected AP beacon TSF.

sl_status_t
sl_wifi_set_roam_configuration(sl_wifi_interface_t interface, const sl_wifi_roam_configuration_t *roam_configuration)

Set the Wi-Fi roaming configuration.

sl_status_t
sl_wifi_get_roam_configuration(sl_wifi_interface_t interface, sl_wifi_roam_configuration_t *roam_configuration)

Get the Wi-Fi roaming configuration.

sl_status_t
sl_wifi_test_client_configuration(sl_wifi_interface_t interface, const sl_wifi_client_configuration_t *ap, uint32_t timeout_ms)

Verify the Wi-Fi client configuration is valid and available.

sl_status_t
sl_wifi_set_certificate(uint8_t certificate_type, const uint8_t *buffer, uint32_t certificate_length)

Load the certificate into the device.

sl_status_t
sl_wifi_set_certificate_with_index(uint8_t certificate_type, uint8_t certificate_index, const uint8_t *buffer, uint32_t certificate_length)

Load the certificate into the device.

sl_status_t
sl_wifi_set_advanced_client_configuration(sl_wifi_interface_t interface, const sl_wifi_advanced_client_configuration_t *configuration)

Set the advanced configuration options of a client interface.

sl_status_t
sl_wifi_configure_timeout(sl_wifi_interface_t interface, sl_wifi_timeout_type_t timeout_type, uint16_t timeout_value)

Configure Wi-Fi timeout parameters.

sl_status_t
sl_wifi_get_timeout(sl_wifi_interface_t interface, sl_wifi_timeout_type_t timeout_type, uint16_t *timeout_value)

Get Wi-Fi timeout parameter value.

sl_status_t
sl_wifi_send_raw_data_frame(sl_wifi_interface_t interface, const void *data, uint16_t data_length)

Send raw data frame.

sl_status_t
sl_wifi_enable_target_wake_time(const sl_wifi_twt_request_t *twt_req)

Configure TWT parameters.

sl_status_t
sl_wifi_disable_target_wake_time(const sl_wifi_twt_request_t *twt_req)

Configure TWT parameters.

sl_status_t
sl_wifi_target_wake_time_auto_selection_v2(const sl_wifi_twt_selection_v2_t *config)

Calculates and configures TWT parameters based on the given inputs.

sl_status_t
sl_wifi_target_wake_time_auto_selection(sl_wifi_twt_selection_t *twt_selection_req) SL_DEPRECATED_API_WISECONNECT_4_1

Calculates and configures TWT parameters based on the given inputs.

sl_status_t
sl_wifi_reschedule_twt(uint8_t flow_id, sl_wifi_reschedule_twt_action_t twt_action, uint64_t suspend_duration)

Suspends the TWT agreement corresponding to given flow id and resumes it when suspend duration expires.

sl_status_t
sl_wifi_filter_broadcast(uint16_t beacon_drop_threshold, uint8_t filter_bcast_in_tim, uint8_t filter_bcast_tim_till_next_cmd) SL_DEPRECATED_API_WISECONNECT_4_1

Send Filter Broadcast Request frame.

sl_status_t
sl_wifi_set_groupcast_filter_config(const sl_wifi_groupcast_filter_config_t *config)

Configure broadcast and multicast filtering on the station interface.

sl_status_t
sl_wifi_allowlist_mcast_add_ip(const sl_ip_address_t *ip_address, sl_ip_address_handle_t *id)

Add an IP multicast address to the NWP allowlist.

sl_status_t
sl_wifi_allowlist_mcast_remove_ip(sl_ip_address_handle_t id)

Remove one multicast allowlist entry by handle.

sl_status_t

Clear the multicast IP allowlist.

sl_status_t
sl_wifi_set_beacon_drop_threshold(sl_wifi_interface_t interface, uint16_t beacon_drop_threshold)

Set the beacon drop threshold used for power save (NWP advanced configuration).

sl_status_t
sl_wifi_get_pairwise_master_key(sl_wifi_interface_t interface, const uint8_t type, const sl_wifi_ssid_t *ssid, const char *pre_shared_key, uint8_t *pairwise_master_key)

Generate PMK if PSK and SSID are provided.

sl_status_t
sl_wifi_configure_multicast_filter(sl_wifi_multicast_filter_info_t *multicast_filter_info) SL_DEPRECATED_API_WISECONNECT_4_1

Configure multicast filter parameters.

Function Documentation#

sl_wifi_connect#

sl_status_t sl_wifi_connect (sl_wifi_interface_t interface, const sl_wifi_client_configuration_t * access_point, uint32_t timeout_ms)

Connect to the given Wi-Fi AP.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi client interface as identified by sl_wifi_interface_t

const sl_wifi_client_configuration_t *[in]access_point

sl_wifi_client_configuration_t object that contains the Access Point details.

uint32_t[in]timeout_ms

Timeout value in milliseconds. The function aborts and returns when the timeout timer expires. A value of 0 indicates an asynchronous action.

  • Pre-conditions:

Returns

Note

  • If security_type is SL_WIFI_WPA3/SL_WIFI_WPA3_ENTERPRISE then SL_WIFI_JOIN_FEAT_MFP_CAPABLE_REQUIRED join feature is enabled internally by SDK. If security_type is SL_WIFI_WPA3_TRANSITION/SL_WIFI_WPA3_TRANSITION_ENTERPRISE then SL_WIFI_JOIN_FEAT_MFP_CAPABLE_REQUIRED join feature is disabled and SL_WIFI_JOIN_FEAT_MFP_CAPABLE_ONLY join feature is enabled internally by SDK. Default Active Channel time is 100 milliseconds. Users can change this default by calling sl_wifi_set_advanced_scan_configuration() before connecting, which allows customization of the active channel scan time for different performance requirements. Default Authentication timeout and Association timeout is 300 milliseconds. If the user wants to modify the time, sl_wifi_set_advanced_client_configuration can be called. Default Keep Alive timeout is 30 seconds. If the user wants to modify the time, sl_wifi_set_advanced_client_configuration can be called.

  • In FCC certified module the behavior is as follows

    1. Region configuration is not supported and if triggered will return error SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE.

    2. STA mode channels 1 to 11 are actively scanned and 12, 13, 14 are passively scanned.

    3. Concurrent mode supports only 1 to 11 channels.

  • For IC parts (non-FCC certified modules), channels 12, 13, and 14 can be actively scanned by setting the device region to a non-US region using sl_si91x_set_device_region API before calling this API.

  • It is recommended to set the timeout to 120000 milliseconds to cover the worst case timeout scenario.

  • If this API fails with error SL_STATUS_TIMEOUT, reset the NWP with sl_net_deinit.


sl_wifi_disconnect#

sl_status_t sl_wifi_disconnect (sl_wifi_interface_t interface)

Disconnect the Wi-Fi client interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi client interface as identified by sl_wifi_interface_t

Returns

Note

  • All si91x, BSD, and IoT sockets associated with the station interface must be closed before invoking this API.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).


sl_wifi_get_signal_strength#

sl_status_t sl_wifi_get_signal_strength (sl_wifi_interface_t interface, int32_t * rssi)

Retrieve the RSSI value of the Access Point to which the Wi-Fi client is connected.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

int32_t *[in]rssi

signal strength (RSSI) in dBm.

Returns

Note

  • The RSSI value is valid only when the Wi-Fi client is connected to an access point. If the Wi-Fi client is disconnected, the RSSI value will be 0xFF.

  • The RSSI value is the average of the last four beacons received by the STA from the connected AP.


sl_wifi_get_ip_config_failure_reason#

sl_status_t sl_wifi_get_ip_config_failure_reason (sl_status_t * ipv4_status, sl_status_t * ipv6_status)

Get the per-family IP configuration status captured during the last IP configuration.

Parameters
TypeDirectionArgument NameDescription
sl_status_t *[out]ipv4_status

Pointer that receives the IPv4 configuration result. May be NULL if not required.

  • SL_STATUS_OK : IPv4 configured successfully

  • firmware error code : IPv4 configuration failed

  • SL_STATUS_NOT_AVAILABLE : IPv4 was not requested in the last attempt

sl_status_t *[out]ipv6_status

Pointer that receives the IPv6 configuration result. May be NULL if not required.

  • SL_STATUS_OK : IPv6 configured successfully

  • firmware error code : IPv6 configuration failed

  • SL_STATUS_NOT_AVAILABLE : IPv6 was not requested in the last attempt

When (IPv4 + IPv6) is brought up and only one family configures successfully, sl_net_up / sl_si91x_configure_ip_address returns a partial-success code (SL_STATUS_WIFI_IPV4_OK or SL_STATUS_WIFI_IPV6_OK). This API lets the application retrieve the underlying per-family result so it can decide how to handle the partially configured link.

When a dual-stack request fails for both families, the return code from sl_net_up or sl_si91x_configure_ip_address contains only the IPv4 failure. Use this API to obtain the IPv6 failure as well.

Returns


sl_wifi_get_sta_tsf#

sl_status_t sl_wifi_get_sta_tsf (sl_wifi_interface_t interface, sl_wifi_tsf64_t * tsf)

Get the station Timing Synchronization Function (TSF) time which is synchronised with connected AP beacon TSF.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

sl_wifi_tsf64_t *[out]tsf

64-bit TSF time in microseconds stored in sl_wifi_tsf64_t structure.

Returns

Note

  • This API returns an error if the station is not connected to an Access Point or at least one beacon is not received.


sl_wifi_set_roam_configuration#

sl_status_t sl_wifi_set_roam_configuration (sl_wifi_interface_t interface, const sl_wifi_roam_configuration_t * roam_configuration)

Set the Wi-Fi roaming configuration.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_roam_configuration_t *[in]roam_configuration

sl_wifi_roam_configuration_t object to store Wi-Fi roaming configuration.

Returns

Note

  • For si91x chips, following ranges are valid: trigger_level: [-10, -100] , trigger_level_change: [0, 90]


sl_wifi_get_roam_configuration#

sl_status_t sl_wifi_get_roam_configuration (sl_wifi_interface_t interface, sl_wifi_roam_configuration_t * roam_configuration)

Get the Wi-Fi roaming configuration.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

sl_wifi_roam_configuration_t *[out]roam_configuration

sl_wifi_roam_configuration_t object that will contain the current roam configuration.

Returns

Note

  • This API is not yet implemented.


sl_wifi_test_client_configuration#

sl_status_t sl_wifi_test_client_configuration (sl_wifi_interface_t interface, const sl_wifi_client_configuration_t * ap, uint32_t timeout_ms)

Verify the Wi-Fi client configuration is valid and available.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_client_configuration_t *[in]ap

sl_wifi_client_configuration_t object that contains the details of Access Point.

uint32_t[in]timeout_ms

Timeout value in milliseconds. The function aborts and returns when the timeout timer expires. A timeout value of 0 means the function initiates the verification process and return immediately, without waiting for the process to complete. This indicates that the action would be handled asynchronously.

  • Pre-conditions:

Returns


sl_wifi_set_certificate#

sl_status_t sl_wifi_set_certificate (uint8_t certificate_type, const uint8_t * buffer, uint32_t certificate_length)

Load the certificate into the device.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]certificate_type

Certificate type being set

const uint8_t *[in]buffer

Pointer to buffer containing the certificate.

uint32_t[in]certificate_length

Length of certificate buffer data.

  • Pre-conditions:

Returns


sl_wifi_set_certificate_with_index#

sl_status_t sl_wifi_set_certificate_with_index (uint8_t certificate_type, uint8_t certificate_index, const uint8_t * buffer, uint32_t certificate_length)

Load the certificate into the device.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]certificate_type

Certificate type being set.

uint8_t[in]certificate_index

Certificate to be loaded in specified index.

const uint8_t *[in]buffer

Pointer to buffer containing the certificate.

uint32_t[in]certificate_length

Length of certificate buffer data.

  • Pre-conditions:

Returns


sl_wifi_set_advanced_client_configuration#

sl_status_t sl_wifi_set_advanced_client_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_client_configuration_t * configuration)

Set the advanced configuration options of a client interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_advanced_client_configuration_t *[in]configuration

Wi-Fi client advanced configuration. See sl_wifi_advanced_client_configuration_t

  • Pre-conditions:

Returns


sl_wifi_configure_timeout#

sl_status_t sl_wifi_configure_timeout (sl_wifi_interface_t interface, sl_wifi_timeout_type_t timeout_type, uint16_t timeout_value)

Configure Wi-Fi timeout parameters.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t.

sl_wifi_timeout_type_t[in]timeout_type

Identifies which timeout type to set. See sl_wifi_timeout_type_t.

uint16_t[in]timeout_value

The timeout value to set. The time resolution depends on the timeout_type:

  • SL_WIFI_AUTHENTICATION_ASSOCIATION_TIMEOUT: milliseconds

  • SL_WIFI_CHANNEL_ACTIVE_SCAN_TIMEOUT: milliseconds

  • SL_WIFI_KEEP_ALIVE_TIMEOUT: seconds

  • SL_WIFI_CHANNEL_PASSIVE_SCAN_TIMEOUT: milliseconds

  • SL_WIFI_BSS_MAX_IDLE_PERIOD: seconds

This API configures various timeout settings for the Wi-Fi module including authentication/association timeout, channel scan timeouts, keep alive timeout, and BSS Max Idle Period. The timeout type determines which parameter is being configured.

For BSS Max Idle Period (SL_WIFI_BSS_MAX_IDLE_PERIOD), this allows the IoT client device to negotiate a longer idle period with the AP, reducing the frequency of keepalive messages for improved power efficiency.

Returns

Note

  • For BSS_MAX_IDLE_PERIOD: can be called after opermode set and before association.

  • Configuration is applied during the next association/reconnection.


sl_wifi_get_timeout#

sl_status_t sl_wifi_get_timeout (sl_wifi_interface_t interface, sl_wifi_timeout_type_t timeout_type, uint16_t * timeout_value)

Get Wi-Fi timeout parameter value.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t.

sl_wifi_timeout_type_t[in]timeout_type

Identifies which timeout value to retrieve. See sl_wifi_timeout_type_t.

uint16_t *[out]timeout_value

Pointer to store the retrieved timeout value.

This API queries timeout parameter values from NWP. For BSS Max Idle Period (SL_WIFI_BSS_MAX_IDLE_PERIOD), it returns the negotiated value from the AP after a successful association.

  • sl_wifi_init should be called before this API. For SL_WIFI_BSS_MAX_IDLE_PERIOD, an active connection to an AP is required.

Returns

Note

  • For BSS Max Idle configuration, the AP may indicate whether keepalive frames must be secured or non-secured. The firmware logs this frame type information, which can be accessed if the application has enabled logging.


sl_wifi_send_raw_data_frame#

sl_status_t sl_wifi_send_raw_data_frame (sl_wifi_interface_t interface, const void * data, uint16_t data_length)

Send raw data frame.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const void *[in]data

Data buffer.

uint16_t[in]data_length

length of the data.

  • Pre-conditions:

    • sl_wifi_init should be called before this API.

    • This API should be invoked only after the module has established a connection in STA or AP mode.

Returns


sl_wifi_enable_target_wake_time#

sl_status_t sl_wifi_enable_target_wake_time (const sl_wifi_twt_request_t * twt_req)

Configure TWT parameters.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_twt_request_t *[in]twt_req

Configurable TWT parameters specified in sl_wifi_twt_request_t.

Enables a TWT session. This is blocking API.

Returns


sl_wifi_disable_target_wake_time#

sl_status_t sl_wifi_disable_target_wake_time (const sl_wifi_twt_request_t * twt_req)

Configure TWT parameters.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_twt_request_t *[in]twt_req

Configurable TWT parameters specified in sl_wifi_twt_request_t.

Disables a TWT session. This is blocking API.

Returns


sl_wifi_target_wake_time_auto_selection_v2#

sl_status_t sl_wifi_target_wake_time_auto_selection_v2 (const sl_wifi_twt_selection_v2_t * config)

Calculates and configures TWT parameters based on the given inputs.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_twt_selection_v2_t *[in]config

sl_wifi_twt_selection_v2_t object containing configurable TWT selection parameters.

Enables or disables a TWT session. This is blocking API.

Returns


sl_wifi_target_wake_time_auto_selection#

sl_status_t sl_wifi_target_wake_time_auto_selection (sl_wifi_twt_selection_t * twt_selection_req)

Calculates and configures TWT parameters based on the given inputs.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_twt_selection_t *[in]twt_selection_req

sl_wifi_twt_selection_t object containing configurable TWT selection parameters.

Enables or disables a TWT session. This is blocking API.

DeprecatedUse sl_wifi_target_wake_time_auto_selection_v2 with sl_wifi_twt_selection_v2_t instead. Internal TWT fields in sl_wifi_twt_selection_t are overwritten by the SDK with default values; only twt_enable, average_tx_throughput, tx_latency, and rx_latency are effective. This API is retained for backward compatibility.

Returns


sl_wifi_reschedule_twt#

sl_status_t sl_wifi_reschedule_twt (uint8_t flow_id, sl_wifi_reschedule_twt_action_t twt_action, uint64_t suspend_duration)

Suspends the TWT agreement corresponding to given flow id and resumes it when suspend duration expires.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]flow_id

Flow id of the twt agreement.

sl_wifi_reschedule_twt_action_t[in]twt_action

sl_wifi_reschedule_twt_action_t specifying different actions that can be taken in relation to rescheduling TWT.

uint64_t[in]suspend_duration

Time interval until which twt agreement is suspended, value taken in milliseconds.

This API performs the following actions on TWT agreement: SL_WIFI_SUSPEND_INDEFINITELY, SL_WIFI_RESUME_IMMEDIATELY, SL_WIFI_SUSPEND_FOR_DURATION. Note

  • The reschedule TWT actions are valid till the end of current TWT agreement. If the TWT agreement is terminated (TWT tear down or WLAN disconnection), these actions are not retained. To reapply these actions upon new TWT agreement, the user must re-issue the command.

The table below outlines the valid values for TWT actions and their corresponding suspend durations:#

twt_action

Valid values for suspend duration

SL_WIFI_SUSPEND_INDEFINITELY

0

SL_WIFI_RESUME_IMMEDIATELY

0

SL_WIFI_SUSPEND_FOR_DURATION

1 to 86400000

Returns


sl_wifi_filter_broadcast#

sl_status_t sl_wifi_filter_broadcast (uint16_t beacon_drop_threshold, uint8_t filter_bcast_in_tim, uint8_t filter_bcast_tim_till_next_cmd)

Send Filter Broadcast Request frame.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]beacon_drop_threshold

The amount of time that FW waits to receive full beacon. Default value is 5000 ms.

uint8_t[in]filter_bcast_in_tim

If this bit is set, then from the next dtim any broadcast data pending bit in TIM indicated will be ignored valid values: 0 - 1.

uint8_t[in]filter_bcast_tim_till_next_cmd

0 - filter_bcast_in_tim is valid till disconnect of the STA. 1 - filter_bcast_in_tim is valid till next update by giving the same command.

DeprecatedDeprecated as of WiSeConnect SDK 4.1.0. Use sl_wifi_set_groupcast_filter_config for broadcast/multicast filtering options and sl_wifi_set_beacon_drop_threshold for the beacon drop threshold; see product documentation for migration from TIM-related fields.

  • Pre-conditions:

Returns

Note


sl_wifi_set_groupcast_filter_config#

sl_status_t sl_wifi_set_groupcast_filter_config (const sl_wifi_groupcast_filter_config_t * config)

Configure broadcast and multicast filtering on the station interface.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_groupcast_filter_config_t *[in]config

Filter enables and mode. See sl_wifi_groupcast_filter_config_t.

  • Pre-conditions:

Returns


sl_wifi_allowlist_mcast_add_ip#

sl_status_t sl_wifi_allowlist_mcast_add_ip (const sl_ip_address_t * ip_address, sl_ip_address_handle_t * id)

Add an IP multicast address to the NWP allowlist.

Parameters
TypeDirectionArgument NameDescription
const sl_ip_address_t *[in]ip_address

IPv4 or IPv6 multicast address to allow.

sl_ip_address_handle_t *[out]id

On success, opaque handle returned by firmware.

Returns a handle for later removal.

  • Pre-conditions:

Returns


sl_wifi_allowlist_mcast_remove_ip#

sl_status_t sl_wifi_allowlist_mcast_remove_ip (sl_ip_address_handle_t id)

Remove one multicast allowlist entry by handle.

Parameters
TypeDirectionArgument NameDescription
sl_ip_address_handle_t[in]id

Handle returned by sl_wifi_allowlist_mcast_add_ip.

  • Pre-conditions:

Returns


sl_wifi_allowlist_mcast_remove_all#

sl_status_t sl_wifi_allowlist_mcast_remove_all (void )

Clear the multicast IP allowlist.

Parameters
TypeDirectionArgument NameDescription
voidN/A
  • Pre-conditions:

Returns


sl_wifi_set_beacon_drop_threshold#

sl_status_t sl_wifi_set_beacon_drop_threshold (sl_wifi_interface_t interface, uint16_t beacon_drop_threshold)

Set the beacon drop threshold used for power save (NWP advanced configuration).

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Client interface that is up and matches the active band configuration.

uint16_t[in]beacon_drop_threshold

Threshold value; valid range is product- and firmware-specific.

For migration, this supersedes the beacon threshold aspect of deprecated sl_wifi_filter_broadcast; TIM-related broadcast filtering is configured separately via sl_wifi_set_groupcast_filter_config.

  • Pre-conditions:

Returns


sl_wifi_get_pairwise_master_key#

sl_status_t sl_wifi_get_pairwise_master_key (sl_wifi_interface_t interface, const uint8_t type, const sl_wifi_ssid_t * ssid, const char * pre_shared_key, uint8_t * pairwise_master_key)

Generate PMK if PSK and SSID are provided.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const uint8_t[in]type

Possible values of this field are 1, 2, and 3, but we only pass 3 for generation of PMK.

const sl_wifi_ssid_t *[in]ssid

SSID of type sl_wifi_ssid_t has the SSID of the access point

const char *[in]pre_shared_key

Expected parameters are pre-shared key(PSK) of the access point

uint8_t *[in]pairwise_master_key

PMK array

This is a blocking API.

Returns


sl_wifi_configure_multicast_filter#

sl_status_t sl_wifi_configure_multicast_filter (sl_wifi_multicast_filter_info_t * multicast_filter_info)

Configure multicast filter parameters.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_multicast_filter_info_t *[in]multicast_filter_info

Configurable multicast filter parameters specified in sl_wifi_multicast_filter_info_t.

This is a blocking API.

DeprecatedDeprecated as of WiSeConnect SDK 4.1.0. Use sl_wifi_set_groupcast_filter_config and the multicast IP allowlist APIs (sl_wifi_allowlist_mcast_add_ip and related) as described in product documentation.

  • Pre-conditions:

Returns

Note