Wi-Fi Credential#
Functions#
Store a credential in specified credential identifier.
Retrieve a stored credential.
Delete a stored credential.
Function Documentation#
sl_wifi_set_credential#
sl_status_t sl_wifi_set_credential (sl_wifi_credential_id_t id, sl_wifi_credential_type_t type, const void * credential, uint32_t credential_length)
Store a credential in specified credential identifier.
[in] | id | Credential identifier as identified by sl_wifi_credential_id_t. |
[in] | type | Credential type as identified by sl_wifi_credential_type_t. |
[in] | credential | Pointer to the credential data object. |
[in] | credential_length | Length of the credential data object. |
This function stores the credential type and data for the specified credential ID. The credential data can include client credentials, access point credentials and user credentials (user credential is a generic credential identifier that can be configured to represent a specific credential type, such as TLS, MQTT, or HTTP, based on the chosen protocol).
Repeatedly calling this API with the same ID will overwrite the existing credential type and data.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
68
of file components/protocol/wifi/inc/sl_wifi_credentials.h
sl_wifi_get_credential#
sl_status_t sl_wifi_get_credential (sl_wifi_credential_id_t id, sl_wifi_credential_type_t * type, void * credential, uint32_t * credential_length)
Retrieve a stored credential.
[in] | id | Credential identifier as identified by sl_wifi_credential_id_t. |
[out] | type | Credential type as identified by sl_wifi_credential_type_t. |
[out] | credential | Pointer to location where credential data is stored. |
[inout] | credential_length | in: Number of bytes available at credential. out: Number of bytes written. |
This function retrieves the credential data for the specified credential ID. The retrieved credential data is stored in the provided credential object.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
100
of file components/protocol/wifi/inc/sl_wifi_credentials.h
sl_wifi_delete_credential#
sl_status_t sl_wifi_delete_credential (sl_wifi_credential_id_t id)
Delete a stored credential.
[in] | id | Credential identifier as identified by sl_wifi_credential_id_t. |
This function deletes the credential data for the specific credential ID and type. Once deleted, the credential cannot be used further for any operations.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
123
of file components/protocol/wifi/inc/sl_wifi_credentials.h