MAC statistics.
Public Attributes#
Current number of frames in the MAC transmission queue.
Highest number of frames in the MAC transmission queue.
Number of successfully received MAC frames.
Number of transmitted MAC frames.
Number of successfully received broadcast MAC frames.
Number of transmitted broadcast MAC frames.
Number of successfully received MAC frames discarded during processing.
Amount of transmitted MAC data in bytes. FCS is not included.
Amount of successfully received MAC data in bytes. FCS is not included.
Number of failed MAC transmissions.
Number of retried MAC transmissions.
Number of MAC CCA attempts.
Number of failed MAC transmissions due to CCA.
Public Attribute Documentation#
tx_queue_size#
uint16_t sl_wisun_statistics_mac_t::tx_queue_size
Current number of frames in the MAC transmission queue.
292
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
tx_queue_peak#
uint16_t sl_wisun_statistics_mac_t::tx_queue_peak
Highest number of frames in the MAC transmission queue.
294
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
rx_count#
uint32_t sl_wisun_statistics_mac_t::rx_count
Number of successfully received MAC frames.
296
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
tx_count#
uint32_t sl_wisun_statistics_mac_t::tx_count
Number of transmitted MAC frames.
298
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
bc_rx_count#
uint32_t sl_wisun_statistics_mac_t::bc_rx_count
Number of successfully received broadcast MAC frames.
300
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
bc_tx_count#
uint32_t sl_wisun_statistics_mac_t::bc_tx_count
Number of transmitted broadcast MAC frames.
302
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
rx_drop_count#
uint32_t sl_wisun_statistics_mac_t::rx_drop_count
Number of successfully received MAC frames discarded during processing.
304
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
tx_bytes#
uint32_t sl_wisun_statistics_mac_t::tx_bytes
Amount of transmitted MAC data in bytes. FCS is not included.
306
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
rx_bytes#
uint32_t sl_wisun_statistics_mac_t::rx_bytes
Amount of successfully received MAC data in bytes. FCS is not included.
308
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
tx_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_failed_count
Number of failed MAC transmissions.
310
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
retry_count#
uint32_t sl_wisun_statistics_mac_t::retry_count
Number of retried MAC transmissions.
312
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
cca_attempts_count#
uint32_t sl_wisun_statistics_mac_t::cca_attempts_count
Number of MAC CCA attempts.
314
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h
failed_cca_count#
uint32_t sl_wisun_statistics_mac_t::failed_cca_count
Number of failed MAC transmissions due to CCA.
316
of file /mnt/raid/workspaces/ws.zJeaRLJo0/overlay/super/protocol/wisun/wisun/inc/sl_wisun_types.h