iPerf server header

Public Attributes#

int32_t

Server flag.

uint32_t

Tot bytes rx'd hi part.

uint32_t

Tot bytes rx'd low part.

uint32_t

Stop time in sec.

uint32_t

Stop time in usec.

uint32_t

Lost pkt cnt.

uint32_t

Rx pkt out of order cnt.

uint32_t

Packet count.

uint32_t

Jitter hi.

uint32_t

Jitter low.

Public Attribute Documentation#

dtg#

sl_iperf_udp_datagram_t sl_iperf_udp_srv_hdr::dtg

Udp datagram.


Definition at line 317 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

flags#

int32_t sl_iperf_udp_srv_hdr::flags

Server flag.


Definition at line 319 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

tot_len_u#

uint32_t sl_iperf_udp_srv_hdr::tot_len_u

Tot bytes rx'd hi part.


Definition at line 321 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

tot_len_l#

uint32_t sl_iperf_udp_srv_hdr::tot_len_l

Tot bytes rx'd low part.


Definition at line 323 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

stop_sec#

uint32_t sl_iperf_udp_srv_hdr::stop_sec

Stop time in sec.


Definition at line 325 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

stop_usec#

uint32_t sl_iperf_udp_srv_hdr::stop_usec

Stop time in usec.


Definition at line 327 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

lost_pkt_cnt#

uint32_t sl_iperf_udp_srv_hdr::lost_pkt_cnt

Lost pkt cnt.


Definition at line 329 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

out_of_order_cnt#

uint32_t sl_iperf_udp_srv_hdr::out_of_order_cnt

Rx pkt out of order cnt.


Definition at line 331 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

packet_cnt#

uint32_t sl_iperf_udp_srv_hdr::packet_cnt

Packet count.


Definition at line 333 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

jitter_sec#

uint32_t sl_iperf_udp_srv_hdr::jitter_sec

Jitter hi.


Definition at line 335 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

jitter_usec#

uint32_t sl_iperf_udp_srv_hdr::jitter_usec

Jitter low.


Definition at line 337 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h