Util Functions#
The Util Functions component provides helper functions to inform the application about the Wi-SUN PHY configured in the RAIL configuration file.
Functions#
Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.
Get PHY settings of the first RAIL configuration listed in RAIL's channelConfigs array.
Connect to a Wi-SUN network.
Function Documentation#
sl_wisun_util_get_rf_settings#
sl_status_t sl_wisun_util_get_rf_settings (uint8_t * reg_domain, uint8_t * op_class, uint16_t * op_mode)
Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t * | [out] | reg_domain | Regulatory domain of the Wi-SUN network |
uint8_t * | [out] | op_class | Operational class of the Wi-SUN network |
uint16_t * | [out] | op_mode | Operational mode of the Wi-SUN network |
Returns
SL_STATUS_OK if successful, an error code otherwise
One of the following:
SL_STATUS_OK if successful
SL_STATUS_INVALID_CONFIGURATION if a configuration that cannot be managed by the plugin is used
SL_STATUS_FAIL if an other error occured
Warnings
Do not call this function while the Wi-SUN stack is started.
DeprecatedThis function will be removed in the future versions of the Wi-SUN stack. See sl_wisun_util_get_phy_config() for a replacement.
62
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_util.h
sl_wisun_util_get_phy_config#
sl_status_t sl_wisun_util_get_phy_config (sl_wisun_phy_config_t * phy_config)
Get PHY settings of the first RAIL configuration listed in RAIL's channelConfigs array.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_wisun_phy_config_t * | [out] | phy_config | Pointer to PHY configuration |
Returns
SL_STATUS_OK if successful, an error code otherwise
One of the following:
SL_STATUS_OK if successful
SL_STATUS_INVALID_CONFIGURATION if a configuration that cannot be managed by the plugin is used
SL_STATUS_FAIL if an other error occured
Warnings
Do not call this function while the Wi-SUN stack is started.
79
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_util.h
sl_wisun_util_connect#
sl_status_t sl_wisun_util_connect (const uint8_t * network_name)
Connect to a Wi-SUN network.
Type | Direction | Argument Name | Description |
---|---|---|---|
const uint8_t * | [in] | network_name | Name of the Wi-SUN network as a zero-terminated string |
Returns
SL_STATUS_OK if successful, an error code otherwise
One of the following:
SL_STATUS_OK if successful
SL_STATUS_INVALID_CONFIGURATION if a configuration that cannot be managed by the plugin is used
SL_STATUS_FAIL if an other error occured
Since Wi-SUN frequency band settings are deduced from first RAIL configuration listed in RAIL's channelConfigs array, using this function is not recommended if more than one RAIL configuration is described.
97
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_util.h