PHY configuration.

Public Attribute Documentation#

type#

uint32_t sl_wisun_phy_config_t::type

Configuration type (sl_wisun_phy_config_type_t)


Definition at line 608 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

fan10#

sl_wisun_phy_config_fan10_t sl_wisun_phy_config_t::fan10

Configuration for SL_WISUN_PHY_CONFIG_FAN10 type.


Definition at line 612 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

fan11#

sl_wisun_phy_config_fan11_t sl_wisun_phy_config_t::fan11

Configuration for SL_WISUN_PHY_CONFIG_FAN11 type.


Definition at line 614 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

explicit_plan#

sl_wisun_phy_config_explicit_t sl_wisun_phy_config_t::explicit_plan

Configuration for SL_WISUN_PHY_CONFIG_EXPLICIT type.


Definition at line 616 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

ids#

sl_wisun_phy_config_ids_t sl_wisun_phy_config_t::ids

Configuration for SL_WISUN_PHY_CONFIG_IDS type.


Definition at line 618 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

custom_fsk#

sl_wisun_phy_config_custom_fsk_t sl_wisun_phy_config_t::custom_fsk

Configuration for SL_WISUN_PHY_CONFIG_CUSTOM_FSK type.


Definition at line 620 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

custom_ofdm#

sl_wisun_phy_config_custom_ofdm_t sl_wisun_phy_config_t::custom_ofdm

Configuration for SL_WISUN_PHY_CONFIG_CUSTOM_OFDM type.


Definition at line 622 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

custom_oqpsk#

sl_wisun_phy_config_custom_oqpsk_t sl_wisun_phy_config_t::custom_oqpsk

Configuration for SL_WISUN_PHY_CONFIG_CUSTOM_OQPSK type.


Definition at line 624 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

config#

union sl_wisun_phy_config_t::@1 sl_wisun_phy_config_t::config

Configuration.


Definition at line 625 of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h