LFN data layer parameters.
Public Attributes#
Initial LFN Unicast interval proposed by the LFN (milliseconds).
Minimum acceptable LFN unicast interval (milliseconds)
Maximum acceptable LFN unicast interval (milliseconds)
The LFN assumes its parent is lost after [lfn_maintain_parent_time] number of Broadcast sync periods with no message received from its parent.
Reserved, set to zero.
Public Attribute Documentation#
unicast_interval_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_ms
Initial LFN Unicast interval proposed by the LFN (milliseconds).
The real unicast interval duration is negotiated with the LFN parent, between unicast_interval_min_ms and unicast_interval_max_ms.
unicast_interval_min_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_min_ms
Minimum acceptable LFN unicast interval (milliseconds)
unicast_interval_max_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_max_ms
Maximum acceptable LFN unicast interval (milliseconds)
lfn_maintain_parent_time#
uint8_t sl_wisun_lfn_params_data_layer_t::lfn_maintain_parent_time
The LFN assumes its parent is lost after [lfn_maintain_parent_time] number of Broadcast sync periods with no message received from its parent.
Specification range [1, 60]