LFN network parameters.
Public Attributes#
uint16_t
Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).
uint8_t
Duration for which an LFN waits for a registration confirmation (minutes).
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
lfn_registration_lifetime_m#
uint16_t sl_wisun_lfn_params_network_t::lfn_registration_lifetime_m
Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).
Specification range [1440, 5040]
lfn_na_wait_duration_m#
uint8_t sl_wisun_lfn_params_network_t::lfn_na_wait_duration_m
Duration for which an LFN waits for a registration confirmation (minutes).
Specification range [30, 120]