MPL parameter set.
Public Attributes#
MPL trickle timer.
uint16_t
MPL seed set entry lifetime (seconds)
uint8_t
MPL trickle timer expirations.
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
trickle#
sl_wisun_trickle_params_t sl_wisun_params_mpl::trickle
MPL trickle timer.
Definition at line
159
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
seed_set_entry_lifetime_s#
uint16_t sl_wisun_params_mpl::seed_set_entry_lifetime_s
MPL seed set entry lifetime (seconds)
Definition at line
161
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle_expirations#
uint8_t sl_wisun_params_mpl::trickle_expirations
MPL trickle timer expirations.
Definition at line
163
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
reserved#
uint8_t sl_wisun_params_mpl::reserved
Reserved, set to zero.
Definition at line
165
of file /mnt/raid/workspaces/ws.3mvRcZlJ0/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h