iPerf log type definition

Public Attributes#

bool

Colored.

bool

Buffered.

int32_t

Last result.

int32_t(*

Stdout and buffer printer.

Buff string instance.

Public Attribute Documentation#

colored#

bool sl_iperf_log::colored

Colored.


Definition at line 259 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

buffered#

bool sl_iperf_log::buffered

Buffered.


Definition at line 261 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

last_res#

int32_t sl_iperf_log::last_res

Last result.


Definition at line 263 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

print#

int32_t(* sl_iperf_log::print) (struct sl_iperf_log *const log, const char *format,...)

Stdout and buffer printer.


Definition at line 265 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

buff#

sl_iperf_log_str_buff_t sl_iperf_log::buff

Buff string instance.


Definition at line 267 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h