iPerf server header
Public Attributes#
Udp datagram.
int32_t
Server flag.
uint32_t
Tot bytes rx'd hi part.
uint32_t
Tot bytes rx'd low part.
uint32_t
Stop time in sec.
uint32_t
Stop time in usec.
uint32_t
Lost pkt cnt.
uint32_t
Rx pkt out of order cnt.
uint32_t
Packet count.
uint32_t
Jitter hi.
uint32_t
Jitter low.
Public Attribute Documentation#
dtg#
sl_iperf_udp_datagram_t sl_iperf_udp_srv_hdr::dtg
Udp datagram.
Definition at line
314
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
flags#
int32_t sl_iperf_udp_srv_hdr::flags
Server flag.
Definition at line
316
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
tot_len_u#
uint32_t sl_iperf_udp_srv_hdr::tot_len_u
Tot bytes rx'd hi part.
Definition at line
318
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
tot_len_l#
uint32_t sl_iperf_udp_srv_hdr::tot_len_l
Tot bytes rx'd low part.
Definition at line
320
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
stop_sec#
uint32_t sl_iperf_udp_srv_hdr::stop_sec
Stop time in sec.
Definition at line
322
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
stop_usec#
uint32_t sl_iperf_udp_srv_hdr::stop_usec
Stop time in usec.
Definition at line
324
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
lost_pkt_cnt#
uint32_t sl_iperf_udp_srv_hdr::lost_pkt_cnt
Lost pkt cnt.
Definition at line
326
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
out_of_order_cnt#
uint32_t sl_iperf_udp_srv_hdr::out_of_order_cnt
Rx pkt out of order cnt.
Definition at line
328
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
packet_cnt#
uint32_t sl_iperf_udp_srv_hdr::packet_cnt
Packet count.
Definition at line
330
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
jitter_sec#
uint32_t sl_iperf_udp_srv_hdr::jitter_sec
Jitter hi.
Definition at line
332
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
jitter_usec#
uint32_t sl_iperf_udp_srv_hdr::jitter_usec
Jitter low.
Definition at line
334
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h