MAC statistics.
Public Attributes#
Current number of frames in the MAC transmission queue.
Highest number of frames in the MAC transmission queue.
Number of successfully received MAC frames.
Number of transmitted MAC frames.
Number of successfully received broadcast MAC frames.
Number of transmitted broadcast MAC frames.
Number of successfully received MAC frames discarded during processing.
Amount of transmitted MAC data in bytes. FCS is not included.
Amount of successfully received MAC data in bytes. FCS is not included.
Number of failed MAC transmissions.
Number of retried MAC transmissions.
Number of MAC CCA attempts.
Number of failed MAC transmissions due to CCA.
Number of successfully received MAC frames using mode_switch.
Number of transmitted MAC frames using mode switch.
Number of failed reception using mode switch (no data after PHR or MDR Command).
Number of failed MAC frames transmission using mode switch.
Public Attribute Documentation#
tx_queue_size#
uint16_t sl_wisun_statistics_mac_t::tx_queue_size
Current number of frames in the MAC transmission queue.
340
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_queue_peak#
uint16_t sl_wisun_statistics_mac_t::tx_queue_peak
Highest number of frames in the MAC transmission queue.
342
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_count#
uint32_t sl_wisun_statistics_mac_t::rx_count
Number of successfully received MAC frames.
344
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_count#
uint32_t sl_wisun_statistics_mac_t::tx_count
Number of transmitted MAC frames.
346
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
bc_rx_count#
uint32_t sl_wisun_statistics_mac_t::bc_rx_count
Number of successfully received broadcast MAC frames.
348
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
bc_tx_count#
uint32_t sl_wisun_statistics_mac_t::bc_tx_count
Number of transmitted broadcast MAC frames.
350
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_drop_count#
uint32_t sl_wisun_statistics_mac_t::rx_drop_count
Number of successfully received MAC frames discarded during processing.
352
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_bytes#
uint32_t sl_wisun_statistics_mac_t::tx_bytes
Amount of transmitted MAC data in bytes. FCS is not included.
354
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_bytes#
uint32_t sl_wisun_statistics_mac_t::rx_bytes
Amount of successfully received MAC data in bytes. FCS is not included.
356
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_failed_count
Number of failed MAC transmissions.
358
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
retry_count#
uint32_t sl_wisun_statistics_mac_t::retry_count
Number of retried MAC transmissions.
360
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
cca_attempts_count#
uint32_t sl_wisun_statistics_mac_t::cca_attempts_count
Number of MAC CCA attempts.
362
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
failed_cca_count#
uint32_t sl_wisun_statistics_mac_t::failed_cca_count
Number of failed MAC transmissions due to CCA.
364
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_count
Number of successfully received MAC frames using mode_switch.
366
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_count
Number of transmitted MAC frames using mode switch.
368
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_failed_count
Number of failed reception using mode switch (no data after PHR or MDR Command).
370
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_failed_count
Number of failed MAC frames transmission using mode switch.
372
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h