Trickle parameters set.
Public Attributes#
uint16_t
Minimum interval size (seconds)
uint16_t
Maximum interval size (seconds)
uint8_t
Redundancy constant (0 for infinity)
Public Attribute Documentation#
imin_s#
uint16_t sl_wisun_trickle_params_t::imin_s
Minimum interval size (seconds)
Definition at line
61
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
imax_s#
uint16_t sl_wisun_trickle_params_t::imax_s
Maximum interval size (seconds)
Definition at line
63
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
k#
uint8_t sl_wisun_trickle_params_t::k
Redundancy constant (0 for infinity)
Definition at line
65
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h