Modules#
iPerf#
The iPerf component provides an iPerf2-compatible solution to measure UDP throughput. It has a full UDP support, and implements a server and client modes, which are capable of sending and receiving packets to measure the bandwidth performance, the inter-arrival jitter, and packet loss.
The component relies on different functions to help configure and run your iPerf test. It allows you to set up your server and client port, your preferred bandwidth, number of packets, remote peer address, and so on. At the end of every iPerf test, an iPerf report is output. Multicast target measurement is supported also. The component can be used with any network stack because it has a portable custom network interface.
To use the iPerf component in your application, add it to your project and initialize it with sl_iperf_service_init().
Functions#
Initialize the iPerf service.
Initialize the iPerf test.
Set the default internal logger for the test descriptor.
Set the default internal test buffer.
Add the iPerf test to the execution queue.
Get the iPerf test from the result queue.
Execute the iPerf UDP client test.
Execute the iPerf UDP server test.
Function Documentation#
sl_iperf_service_init#
void sl_iperf_service_init (void )
Initialize the iPerf service.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Init OS objects and default contents
sl_iperf_test_init#
void sl_iperf_test_init (sl_iperf_test_t *const test, sl_iperf_mode_t mode, sl_iperf_protocol_t protocol)
Initialize the iPerf test.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t *const | [inout] | test | Test descriptor |
| sl_iperf_mode_t | [in] | mode | Mode |
| sl_iperf_protocol_t | [in] | protocol | Protocol |
Initialize a test descriptor with default content
sl_iperf_test_set_default_logger#
void sl_iperf_test_set_default_logger (sl_iperf_test_t *const test)
Set the default internal logger for the test descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t *const | [out] | test | Test descriptor |
Helper function
sl_iperf_test_set_default_buff#
void sl_iperf_test_set_default_buff (sl_iperf_test_t *const test)
Set the default internal test buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t *const | [out] | test | Test descriptor |
Helper function
sl_iperf_test_add#
bool sl_iperf_test_add (sl_iperf_test_t *const test)
Add the iPerf test to the execution queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t *const | [in] | test | Test descriptor |
Add test to the input messagequeue. Returns
true On Success
false On Failure
sl_iperf_test_get#
bool sl_iperf_test_get (sl_iperf_test_t *const test)
Get the iPerf test from the result queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t *const | [out] | test | Destination test descriptor |
Get the test from the output messagequeue. Returns
true On Success
false On Failure
sl_iperf_test_udp_client#
void sl_iperf_test_udp_client (sl_iperf_test_t * test)
Execute the iPerf UDP client test.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t * | [inout] | test | Test descriptor |
iPerf UDP client test.
sl_iperf_test_udp_server#
void sl_iperf_test_udp_server (sl_iperf_test_t * test)
Execute the iPerf UDP server test.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iperf_test_t * | [inout] | test | Test descriptor |
iPerf UDP server test.