Modules#

CoAP type definitions

CoAP#

The Wi-SUN CoAP component provides an application layer implementation on top of the Wi-SUN stack and its socket API. The CoAP protocol is designed as a specialized Internet Application Protocol for constrained devices in lossy networks (see RFC 7252 for additional information). Wi-SUN FAN networks fit this definition. The CoAP implementation relies on the UDP transport layer to send and receive packets.

A number of helper functions are part of the component to help build CoAP payloads, parse CoAP packets, free CoAP packets, and more.

CoAP Resource Handler service handles registered resources. Resource Discovery request provides an interface to get information about available resources. Resource has more attributes over URI (Uniform Resource Identifier) path, which can be filtered by particular Resource Discovery request.

To use the CoAP component in your application, add it to your project and initialize it with sl_wisun_coap_init().

Functions#

bool
sl_wisun_coap_init(const sl_wisun_coap_tx_callback tx_callback, const sl_wisun_coap_rx_callback rx_callback, const sl_wisun_coap_version_t version)

Initialize Wi-SUN CoAP.

__STATIC_INLINE bool

Initialize Wi-SUN CoAP default.

bool

Get lib state.

void *
sl_wisun_coap_malloc(uint16_t size)

Implement malloc.

void
sl_wisun_coap_free(void *addr)

Free Wi-SUN CoAP.

sl_wisun_coap_parser(uint16_t packet_data_len, uint8_t *packet_data)

CoAP parser wrapper function.

uint16_t
sl_wisun_coap_builder_calc_size(const sl_wisun_coap_packet_t *message)

CoAP packet calc size wrapper.

int16_t
sl_wisun_coap_builder(uint8_t *dest_buff, const sl_wisun_coap_packet_t *message)

CoAP message builder Wi-SUN.

sl_wisun_coap_build_response(const sl_wisun_coap_packet_t *req, sl_wisun_coap_message_code_t msg_code)

Build generic response for request wrapper function.

void
sl_wisun_coap_print_packet(const sl_wisun_coap_packet_t *packet, const bool hex_format)

Print CoAP packets and all of attached buffer, payload, token, uri_path.

char *
sl_wisun_coap_get_uri_path_str(const sl_wisun_coap_packet_t *const packet)

Prepare URI path string.

__STATIC_INLINE void

Destroy URI path string.

Get the library handler pointer from the internal handler structure.

void
sl_wisun_coap_destroy_packet(sl_wisun_coap_packet_t *packet)

Destroy packet.

char *
sl_wisun_coap_get_payload_str(const sl_wisun_coap_packet_t *const packet)

Prepare payload string.

__STATIC_INLINE void

Destroy payload string.

Macros#

#define

CoAP Service loop.

Function Documentation#

sl_wisun_coap_init#

bool sl_wisun_coap_init (const sl_wisun_coap_tx_callback tx_callback, const sl_wisun_coap_rx_callback rx_callback, const sl_wisun_coap_version_t version)

Initialize Wi-SUN CoAP.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_tx_callback[in]tx_callback

TX callback, if it's NULL, the default callback is applied

const sl_wisun_coap_rx_callback[in]rx_callback

RX callback, if it's NULL, the default callback is applied

const sl_wisun_coap_version_t[in]version

CoAP version

Set the Wi-SUN CoAP internal descriptor. Returns

  • true Proper initialization

  • false Error


sl_wisun_coap_init_default#

__STATIC_INLINE bool sl_wisun_coap_init_default (void )

Initialize Wi-SUN CoAP default.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initializes the internal descriptor with default values. Returns

  • true Proper initialization

  • false Error


sl_wisun_coap_is_initialized#

bool sl_wisun_coap_is_initialized (void )

Get lib state.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Gets the initialized state of the CoAP library to decide whether the init is needed. Returns

  • true Initialized

  • false Not initialized


sl_wisun_coap_malloc#

void* sl_wisun_coap_malloc (uint16_t size)

Implement malloc.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Asize

size for malloc

OS-dependent thread-safe implementation. Returns

  • void* the memory pointer


sl_wisun_coap_free#

void sl_wisun_coap_free (void * addr)

Free Wi-SUN CoAP.

Parameters
TypeDirectionArgument NameDescription
void *N/Aaddr

address ptr

OS-dependent thread-safe implementation.


sl_wisun_coap_parser#

sl_wisun_coap_packet_t* sl_wisun_coap_parser (uint16_t packet_data_len, uint8_t * packet_data)

CoAP parser wrapper function.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]packet_data_len

packet data size

uint8_t *[in]packet_data

packet data ptr

Used sn_coap_parser Returns

  • sl_wisun_coap_packet_t* Parsed packet pointer


sl_wisun_coap_builder_calc_size#

uint16_t sl_wisun_coap_builder_calc_size (const sl_wisun_coap_packet_t * message)

CoAP packet calc size wrapper.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]message

message ptr

Used sn_coap_builder_calc_needed_packet_data_size. Returns

  • uint16_t size


sl_wisun_coap_builder#

int16_t sl_wisun_coap_builder (uint8_t * dest_buff, const sl_wisun_coap_packet_t * message)

CoAP message builder Wi-SUN.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]dest_buff

destination buffer for raw message

const sl_wisun_coap_packet_t *[in]message

message structure

Used sl_wisun_coap_builder. Returns

  • int16_t On success bytes of built message, on failure -1 if CoAP header structure is wrong -2 if NULL ptr set as argument


sl_wisun_coap_build_response#

sl_wisun_coap_packet_t* sl_wisun_coap_build_response (const sl_wisun_coap_packet_t * req, sl_wisun_coap_message_code_t msg_code)

Build generic response for request wrapper function.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]req

request

sl_wisun_coap_message_code_t[in]msg_code

message code to build

Used sn_coap_build_response. Returns

  • sl_wisun_coap_header_t* built packet ptr on the heap


sl_wisun_coap_print_packet#

void sl_wisun_coap_print_packet (const sl_wisun_coap_packet_t * packet, const bool hex_format)

Print CoAP packets and all of attached buffer, payload, token, uri_path.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *[in]packet

packet to print

const bool[in]hex_format

hex format bool to decide buffer print format

Pretty printer function, with hex format option for buffers


sl_wisun_coap_get_uri_path_str#

char* sl_wisun_coap_get_uri_path_str (const sl_wisun_coap_packet_t *const packet)

Prepare URI path string.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *const[in]packet

Packet

'\0' terminated string in the heap, it must be freed Returns

  • char* URI path string, NULL on error


sl_wisun_coap_destroy_uri_path_str#

__STATIC_INLINE void sl_wisun_coap_destroy_uri_path_str (char * uri_str)

Destroy URI path string.

Parameters
TypeDirectionArgument NameDescription
char *[in]uri_str

URI string ptr

Call free on allocated pointer


sl_wisun_coap_get_lib_handler#

const sl_wisun_coap_handle_t* sl_wisun_coap_get_lib_handler (void )

Get the library handler pointer from the internal handler structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Not thread safe! It is needed only to use Pelion mbed-coap library functions Returns

  • const sl_wisun_coap_handle_t* pointer to the lib handler


sl_wisun_coap_destroy_packet#

void sl_wisun_coap_destroy_packet (sl_wisun_coap_packet_t * packet)

Destroy packet.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_coap_packet_t *N/Apacket

packet

It must be used to avoid memory leaks! Free the all of allocated buffer for packet


sl_wisun_coap_get_payload_str#

char* sl_wisun_coap_get_payload_str (const sl_wisun_coap_packet_t *const packet)

Prepare payload string.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_coap_packet_t *const[in]packet

Packet

'\0' terminated string in the heap, it must be freed Returns

  • char* payload string, NULL on error


sl_wisun_coap_destroy_payload_str#

__STATIC_INLINE void sl_wisun_coap_destroy_payload_str (char * str)

Destroy payload string.

Parameters
TypeDirectionArgument NameDescription
char *[in]str

String

'\0' terminated string in the heap, it must be freed


Macro Definition Documentation#

SL_COAP_SERVICE_LOOP#

#define SL_COAP_SERVICE_LOOP
Value:
()

CoAP Service loop.