iPerf Client Header extended

Public Attributes#

int32_t

Type.

int32_t

Length.

int16_t

Upper flags.

int16_t

Lower flags.

uint32_t

Upper version.

uint32_t

Lower version.

uint16_t

Reserved.

uint16_t

Tos.

uint32_t

Lower rate.

uint32_t

Upper rate.

uint32_t

TCP write prefetch.

Public Attribute Documentation#

type#

int32_t sl_iperf_clnt_hdr_ext::type

Type.


Definition at line 356 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

length#

int32_t sl_iperf_clnt_hdr_ext::length

Length.


Definition at line 358 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_flags#

int16_t sl_iperf_clnt_hdr_ext::u_flags

Upper flags.


Definition at line 360 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_flags#

int16_t sl_iperf_clnt_hdr_ext::l_flags

Lower flags.


Definition at line 362 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_version#

uint32_t sl_iperf_clnt_hdr_ext::u_version

Upper version.


Definition at line 364 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_version#

uint32_t sl_iperf_clnt_hdr_ext::l_version

Lower version.


Definition at line 366 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

reserved#

uint16_t sl_iperf_clnt_hdr_ext::reserved

Reserved.


Definition at line 368 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

tos#

uint16_t sl_iperf_clnt_hdr_ext::tos

Tos.


Definition at line 370 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_rate#

uint32_t sl_iperf_clnt_hdr_ext::l_rate

Lower rate.


Definition at line 372 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_rate#

uint32_t sl_iperf_clnt_hdr_ext::u_rate

Upper rate.


Definition at line 374 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

tcp_write_prefetch#

uint32_t sl_iperf_clnt_hdr_ext::tcp_write_prefetch

TCP write prefetch.


Definition at line 376 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h