Border Router API#

Wi-SUN Border Router API contains functions for Border Router specific functionality.

The API is an extension, not a replacement of Wi-SUN Stack API. An application implementing Border Router capability may utilize functions from both APIs. See API availability for further information.

Functions#

sl_status_t
sl_wisun_br_get_gak(uint8_t index, uint8_t *gak)

Get Group AES Key.

sl_status_t
sl_wisun_br_get_ip_addresses(uint8_t *addr_ll, uint8_t *addr_gua, uint8_t *addr_dodagid)

Get the unicast IPv6 addresses configured in the Border Router.

sl_status_t
sl_wisun_br_get_routing_table(uint16_t *entry_count, sl_wisun_br_routing_table_entry_t *table)

Get the Routing Table.

sl_status_t

Get the Routing Table Size.

sl_status_t
sl_wisun_br_get_routing_table_from_index(uint16_t start_index, uint16_t *entry_count, sl_wisun_br_routing_table_entry_t *entries)

Get the Routing Table starting from a specific index.

sl_status_t
sl_wisun_br_get_state(sl_wisun_br_state_t *state)

Get the Border Router state.

sl_status_t
sl_wisun_br_ipv6_down(const uint8_t *data, size_t data_length)

Forward an IPv6 packet to Wi-SUN network.

sl_status_t
sl_wisun_br_ipv6_route_exists(const uint8_t *ipv6_address, bool *exists)

Check if the IPv6 destination address is routable in the Wi-SUN network.

sl_status_t
sl_wisun_br_pan_defect_advertise(bool defect_advertise, uint32_t min_scan_duration_s, uint32_t max_scan_duration_s)

Start or stop PAN Defect advertisement.

sl_status_t
sl_wisun_br_revoke_gtks(bool revoke_lgtks, const uint8_t *gtk)

Revoke (LFN) Group Transient Keys and installs a new key.

sl_status_t
sl_wisun_br_revoke_pairwise_keys(const sl_wisun_mac_address_t *address)

Remove pairwise keys associated with a node.

sl_status_t
sl_wisun_br_set_broadcast_settings(uint32_t interval_ms, uint8_t dwell_interval_ms)

Set broadcast settings.

sl_status_t
sl_wisun_br_set_connection_parameters(const sl_wisun_br_connection_params_t *params)

Configure the Border Router parameter set.

sl_status_t
sl_wisun_br_set_device_certificate(uint16_t certificate_options, uint16_t certificate_length, const uint8_t *certificate)

Set the Border Router device certificate.

sl_status_t
sl_wisun_br_set_gtk(const uint8_t *gtk, uint8_t index)

Set Group Transient Key.

sl_status_t
sl_wisun_br_set_ipv6_prefix(const uint8_t *ipv6_prefix, uint8_t prefix_length)

Set IPv6 prefix for the Wi-SUN network.

sl_status_t
sl_wisun_br_set_ipv6_up_handler(sl_wisun_ipv6_up_handler_t handler)

Register a function to handle IPv6 packets received from Wi-SUN network.

sl_status_t
sl_wisun_br_set_lfn_parameters(const sl_wisun_br_lfn_params_t *params)

Configure LFN parenting parameter set.

sl_status_t
sl_wisun_br_set_lfn_support(uint8_t lfn_limit, bool lfn_support_pan)

Configure LFN parenting support.

sl_status_t
sl_wisun_br_set_network_size(sl_wisun_network_size_t size)

Set the size of the Wi-SUN network.

sl_status_t
sl_wisun_br_start(const uint8_t *name, const sl_wisun_phy_config_t *phy_config)

Start the Border Router.

sl_status_t

Stop the Border Router.

sl_status_t

Trigger a global repair process from the Border Router.

Macros#

#define
sl_wisun_set_br_device_certificate sl_wisun_br_set_device_certificate

Define sl_wisun_set_br_device_certificate for legacy.

Function Documentation#

sl_wisun_br_get_gak#

sl_status_t sl_wisun_br_get_gak (uint8_t index, uint8_t * gak)

Get Group AES Key.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]index

Index of the key from 0 to 3 for GAKs and 4 to 6 for LFN GAKs

uint8_t *[out]gak

Pointer to Group AES Key

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function exports (L)GAK as a plaintext key.

Note

  • This functionality is only available when using the debug library.


sl_wisun_br_get_ip_addresses#

sl_status_t sl_wisun_br_get_ip_addresses (uint8_t * addr_ll, uint8_t * addr_gua, uint8_t * addr_dodagid)

Get the unicast IPv6 addresses configured in the Border Router.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]addr_ll

Pointer to Link-Local address

uint8_t *[out]addr_gua

Pointer to Unique Local Address or Global Unicast Address

uint8_t *[out]addr_dodagid

Pointer to DODAG ID

Returns

  • SL_STATUS_OK if successful, an error code otherwise


sl_wisun_br_get_routing_table#

sl_status_t sl_wisun_br_get_routing_table (uint16_t * entry_count, sl_wisun_br_routing_table_entry_t * table)

Get the Routing Table.

Parameters
TypeDirectionArgument NameDescription
uint16_t *[inout]entry_count

Maximum number of entries to read on input, number of entries read on output

sl_wisun_br_routing_table_entry_t *[out]table

Pointer to the application allocated memory where the routing table is written

Returns

  • SL_STATUS_OK if successful, an error code otherwise

The routing table is unordered and only contains the parent-child relationship between the nodes. The table is in the format: | Node GUA/ULA 16 bytes | parent GUA/ULA 16 bytes |

Note


sl_wisun_br_get_routing_table_entry_count#

sl_status_t sl_wisun_br_get_routing_table_entry_count (uint16_t * entry_count)

Get the Routing Table Size.

Parameters
TypeDirectionArgument NameDescription
uint16_t *[out]entry_count

Number of entries in the routing table

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function retrieves the number of entries in the routing table. This allows for allocation before calling sl_wisun_br_get_routing_table(). The allocated memory should be at least equal to: sizeof(sl_wisun_br_routing_table_entry_t) * entry_count.


sl_wisun_br_get_routing_table_from_index#

sl_status_t sl_wisun_br_get_routing_table_from_index (uint16_t start_index, uint16_t * entry_count, sl_wisun_br_routing_table_entry_t * entries)

Get the Routing Table starting from a specific index.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]start_index

Index to start reading the routing table from

uint16_t *[inout]entry_count

Maximum number of entries to read on input, number of entries read on output

sl_wisun_br_routing_table_entry_t *[out]entries

Pointer to the application allocated memory where the routing table is written

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function retrieves entry_count entries from the routing table, starting from a specific index. This allows the caller to get any number of entries from the routing table without having to allocate a large buffer. The allocated memory should be at least equal to: sizeof(sl_wisun_br_routing_table_entry_t) * entry_count.

Note

Warnings

  • If the application does not retrieve the entire routing table in a single read, it may miss updates or changes in the network topology.


sl_wisun_br_get_state#

sl_status_t sl_wisun_br_get_state (sl_wisun_br_state_t * state)

Get the Border Router state.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_br_state_t *[out]state

Pointer to state

Returns

  • SL_STATUS_OK if successful, an error code otherwise


sl_wisun_br_ipv6_down#

sl_status_t sl_wisun_br_ipv6_down (const uint8_t * data, size_t data_length)

Forward an IPv6 packet to Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]data

Pointer to IPv6 header

size_t[out]data_length

Length of IPv6 packet data in bytes

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function forwards an IPv6 packet to Wi-SUN network. The destination address must belong to the DODAG prefix. This function is used for handling downlink packets from the backhaul interface, see sl_wisun_br_set_ipv6_up_handler() for uplink. It's recommended to use sl_wisun_br_ipv6_route_exists() before forwarding a packet.


sl_wisun_br_ipv6_route_exists#

sl_status_t sl_wisun_br_ipv6_route_exists (const uint8_t * ipv6_address, bool * exists)

Check if the IPv6 destination address is routable in the Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]ipv6_address

Pointer to IPv6 destination address

bool *[out]exists

Whether the address is routable

  • true: address is routable

  • false: address is not routable

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function checks if the given IPv6 address is a valid destination in the Wi-SUN network. The destination address must belong to the Border Router or one of the connected nodes.


sl_wisun_br_pan_defect_advertise#

sl_status_t sl_wisun_br_pan_defect_advertise (bool defect_advertise, uint32_t min_scan_duration_s, uint32_t max_scan_duration_s)

Start or stop PAN Defect advertisement.

Parameters
TypeDirectionArgument NameDescription
bool[in]defect_advertise

True to start PAN Defect procedure, false to stop it.

uint32_t[in]min_scan_duration_s

Minimum duration after which devices are allowed to switch their PAN if an alternative one is available.

uint32_t[in]max_scan_duration_s

Duration after which devices should systemically switch to the alternative PAN if one is available.

Returns

  • SL_STATUS_OK if successful, an error code otherwise.

Note

  • The values for min_scan_duration_s and max_scan_duration_s should be chosen based on the estimated performance of the backup power source. Specifically, max_scan_duration_s should be set to a value smaller than the estimated lifetime of the backup power source to ensure a seamless transition to the alternative PAN without long connection interruptions.


sl_wisun_br_revoke_gtks#

sl_status_t sl_wisun_br_revoke_gtks (bool revoke_lgtks, const uint8_t * gtk)

Revoke (LFN) Group Transient Keys and installs a new key.

Parameters
TypeDirectionArgument NameDescription
bool[in]revoke_lgtks

True to revoke LGTKs, false to revoke GTKs

const uint8_t *[in]gtk

(LFN) Group Transient Key

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Destroy all (L)GTKs except the current active one (and potentially the next key), reduce the current (or next) key's lifetime, and add a new key, as described in the Wi-SUN FAN specification section 6.5.2.5.

Note

  • The gtk parameter is provided for test and debug purposes: setting a specific key in production is not recommended. Set to NULL to generate a random key.


sl_wisun_br_revoke_pairwise_keys#

sl_status_t sl_wisun_br_revoke_pairwise_keys (const sl_wisun_mac_address_t * address)

Remove pairwise keys associated with a node.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]address

EUI-64 of the target node

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Remove the Pairwise Transient Key (PTK) and Pairwise Master Key (PMK) associated with a node as described in the Wi-SUN FAN specification section 6.5.2.5.

Note

  • To permanently revoke access to the node, its certificate must be banned at the authentication authority (e.g. RADIUS server).


sl_wisun_br_set_broadcast_settings#

sl_status_t sl_wisun_br_set_broadcast_settings (uint32_t interval_ms, uint8_t dwell_interval_ms)

Set broadcast settings.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]interval_ms

Broadcast Interval (BDI < BI <= 16777215 ms) (default: 1020 ms)

uint8_t[in]dwell_interval_ms

Broadcast Dwell Interval (100-255 ms) (default: 255 ms)

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the broadcast channel hopping schedule. The Broadcast Interval is the duration, between Broadcast Dwell Intervals within the advertising node’s broadcast schedule. Its resolution is limited to 24 bits (16777215 ms). The Broadcast Dwell Interval specifies the duration during which the node may transmit a broadcast message. It is recommended a BI value of 4.0 times the maximum of (UDI, BDI). These values affect the whole PAN, since they are propagated from parent to children. This function must be called before starting the Border Router.


sl_wisun_br_set_connection_parameters#

sl_status_t sl_wisun_br_set_connection_parameters (const sl_wisun_br_connection_params_t * params)

Configure the Border Router parameter set.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_br_connection_params_t *[in]params

Parameter set to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This functions sets the Border Router parameter set. These parameters impact connection time, bandwidth usage, and latency. Use of a predefined parameter set is recommended (Predefined BR parameter sets). Small profile will be used by default for all missing configurations. This function must be called before starting the Border Router.


sl_wisun_br_set_device_certificate#

sl_status_t sl_wisun_br_set_device_certificate (uint16_t certificate_options, uint16_t certificate_length, const uint8_t * certificate)

Set the Border Router device certificate.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]certificate_options

Options for the certificate.
SL_WISUN_CERTIFICATE_OPTION_APPEND: Append the certificate to the list of server certificates instead of replacing the previous entries
SL_WISUN_CERTIFICATE_OPTION_IS_REF: The application guarantees the certificate data will remain in scope and can therefore be referenced instead of copied
SL_WISUN_CERTIFICATE_OPTION_HAS_KEY: The certificate has a private key

uint16_t[in]certificate_length

Size of the certificate data

const uint8_t *[in]certificate

Pointer to the certificate data

Returns

  • SL_STATUS_OK if successful, an error code otherwise


sl_wisun_br_set_gtk#

sl_status_t sl_wisun_br_set_gtk (const uint8_t * gtk, uint8_t index)

Set Group Transient Key.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]gtk

Group Transient Key

uint8_t[in]index

Index of the key from 0 to 3 for GTKs and 4 to 6 for LGTKs

Note

  • This API is provided for test and debug purposes: setting a specific key in production is not recommended. The keys set using this API are saved to NVM, and subsequent calls to this API are ignored until the NVM is cleared using sl_wisun_clear_credential_cache.

Returns

  • SL_STATUS_OK if successful, SL_STATUS_ALREADY_EXISTS when ignored, an error code otherwise


sl_wisun_br_set_ipv6_prefix#

sl_status_t sl_wisun_br_set_ipv6_prefix (const uint8_t * ipv6_prefix, uint8_t prefix_length)

Set IPv6 prefix for the Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]ipv6_prefix

IPv6 prefix

uint8_t[in]prefix_length

Prefix length. Currently, only 64 bit prefixes are supported.

Note

  • Must not be called after the border router is started

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the prefix used to generate IP addresses for RPL traffic (DODAGID will derive from it). This function must be called before starting the Border Router.


sl_wisun_br_set_ipv6_up_handler#

sl_status_t sl_wisun_br_set_ipv6_up_handler (sl_wisun_ipv6_up_handler_t handler)

Register a function to handle IPv6 packets received from Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_ipv6_up_handler_t[in]handler

Pointer to handler function

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function registers a handler function that will be called when the destination address of a received IPv6 packet is outside the DODAG prefix. Setting the handler function to NULL disables the forwarding. This function is used for handling uplink packets towards the backhaul interface, see sl_wisun_br_ipv6_down() for downlink.


sl_wisun_br_set_lfn_parameters#

sl_status_t sl_wisun_br_set_lfn_parameters (const sl_wisun_br_lfn_params_t * params)

Configure LFN parenting parameter set.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_br_lfn_params_t *[in]params

Parameter set to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the LFN parenting parameter set. These parameters impact battery life of all LFNs in the PAN. Use of a predefined parameter set is recommended (Predefined BR LFN-parenting parameter sets). This function must be called before starting the Border Router.


sl_wisun_br_set_lfn_support#

sl_status_t sl_wisun_br_set_lfn_support (uint8_t lfn_limit, bool lfn_support_pan)

Configure LFN parenting support.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]lfn_limit

Maximum number of LFN children

  • 0: LFN parenting is disabled in the Border Router

  • **> 0**: Maximum number of LFN children the Border Router can parent

bool[in]lfn_support_pan

LFN parenting support in the PAN

  • true: LFN parenting is enabled in the PAN

  • false: LFN parenting is disabled in the PAN

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function configures LFN parenting support in the Border Router and in the PAN. Set sl_wisun_config_neighbor_table accordingly.


sl_wisun_br_set_network_size#

sl_status_t sl_wisun_br_set_network_size (sl_wisun_network_size_t size)

Set the size of the Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_network_size_t[in]size

Size of the network
SL_WISUN_NETWORK_SIZE_AUTOMATIC: network size is managed automatically
SL_WISUN_NETWORK_SIZE_SMALL: less than 100 nodes
SL_WISUN_NETWORK_SIZE_MEDIUM: 100 to 800 nodes
SL_WISUN_NETWORK_SIZE_LARGE: 800 to 1500 nodes

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the size of the network. The size is used to set various stack parameters, such as timing parameters to optimize device behavior in regards to node count. The device will function with any setting but may exhibit non-optimal behavior. Setting the size too large may cause slow connection speed and increased latency. Conversely, a value too small may cause increased network traffic.


sl_wisun_br_start#

sl_status_t sl_wisun_br_start (const uint8_t * name, const sl_wisun_phy_config_t * phy_config)

Start the Border Router.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]name

Name of the Wi-SUN network as a zero-terminated string

const sl_wisun_phy_config_t *[in]phy_config

Pointer to PHY configuration

Returns

  • SL_STATUS_OK if successful, an error code otherwise


sl_wisun_br_stop#

sl_status_t sl_wisun_br_stop (void )

Stop the Border Router.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • SL_STATUS_OK if successful, an error code otherwise


sl_wisun_br_trigger_global_repair#

sl_status_t sl_wisun_br_trigger_global_repair (void )

Trigger a global repair process from the Border Router.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • SL_STATUS_OK if successful SL_STATUS_NOT_READY if the Border Router is not started SL_STATUS_FAIL if the DODAG Version is not incremented

Increments the RPL DODAG Version to allow nodes in the network to choose a new position whose rank is not constrained by their rank within the old DODAG Version. The new DODAG Version is propagated through DIOs in the entire network and will cause all nodes to re-run a parent selection within the new DODAG Version, effectively temporarily disconnecting them from the network.

Note

  • This operation will disrupt network communications as the repair process is carried out. It is not recommended to trigger a global repair more often than once every 24 hours.