You are viewing documentation for version:2.10.0PDFMAC address. Public Attributes#uint8_taddressMAC address. Public Attribute Documentation#address#uint8_t sl_wisun_mac_address_t::address[SL_WISUN_MAC_ADDRESS_SIZE]MAC address. This field contains a MAC address (EUI-64) stored in canonical format where the first byte of the array is the most-significant byte of the MAC address.