LFN parameter set.

Public Attributes#

DHCP parameter set.

LFN EAPOL parameters.

MAC parameter set.

LFN network parameters.

LFN power parameters.

Traffic parameter set.

uint32_t

Version of this API.

Public Attribute Documentation#

connection#

sl_wisun_lfn_params_connection_t sl_wisun_lfn_params_t::connection

LFN connection parameters.


data_layer#

sl_wisun_lfn_params_data_layer_t sl_wisun_lfn_params_t::data_layer

LFN data layer parameters.


dhcp#

sl_wisun_params_dhcp_t sl_wisun_lfn_params_t::dhcp

DHCP parameter set.


eapol#

sl_wisun_lfn_params_eapol_t sl_wisun_lfn_params_t::eapol

LFN EAPOL parameters.


mac#

sl_wisun_mac_params_t sl_wisun_lfn_params_t::mac

MAC parameter set.


network#

sl_wisun_lfn_params_network_t sl_wisun_lfn_params_t::network

LFN network parameters.


power#

sl_wisun_lfn_params_power_t sl_wisun_lfn_params_t::power

LFN power parameters.


traffic#

sl_wisun_params_traffic_t sl_wisun_lfn_params_t::traffic

Traffic parameter set.


version#

uint32_t sl_wisun_lfn_params_t::version

Version of this API.

This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.