LFN EAPOL parameters.

Public Attributes#

uint8_t

If true, allow join state 2 to be skipped using cached credentials from the previous connection.

uint16_t

Max delay of first key request (seconds)

uint8_t

Maximum retransmission count.

uint16_t

Maximum duration for retransmissions (seconds)

uint16_t

Initial retransmission time (seconds)

uint16_t

LGTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a LGTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

allow_skip#

uint8_t sl_wisun_lfn_params_eapol_t::allow_skip

If true, allow join state 2 to be skipped using cached credentials from the previous connection.


initial_key_max_s#

uint16_t sl_wisun_lfn_params_eapol_t::initial_key_max_s

Max delay of first key request (seconds)


initial_key_retry_limit#

uint8_t sl_wisun_lfn_params_eapol_t::initial_key_retry_limit

Maximum retransmission count.


initial_key_retry_max_limit_s#

uint16_t sl_wisun_lfn_params_eapol_t::initial_key_retry_max_limit_s

Maximum duration for retransmissions (seconds)


initial_key_retry_min_s#

uint16_t sl_wisun_lfn_params_eapol_t::initial_key_retry_min_s

Initial retransmission time (seconds)


lgtk_max_mismatch_m#

uint16_t sl_wisun_lfn_params_eapol_t::lgtk_max_mismatch_m

LGTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a LGTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.


reserved#

uint8_t sl_wisun_lfn_params_eapol_t::reserved[2]

Reserved, set to zero.