Wi-SUN event definitions.

This structure contains a Wi-SUN API event and its associated data.

Public Attributes#

union sl_wisun_evt_t::@0

Event-specific data.

Common event header.

Public Attribute Documentation#

br_routing_table_update#

sl_wisun_br_msg_routing_table_update_ind_body_t sl_wisun_evt_t::br_routing_table_update

SL_WISUN_BR_MSG_ROUTING_TABLE_UPDATE_IND_ID event data


br_stopped#

sl_wisun_br_msg_stopped_ind_body_t sl_wisun_evt_t::br_stopped

SL_WISUN_BR_MSG_STOPPED_IND_ID event data


connected#

sl_wisun_msg_connected_ind_body_t sl_wisun_evt_t::connected

SL_WISUN_MSG_CONNECTED_IND_ID event data


connection_lost#

sl_wisun_msg_connection_lost_ind_body_t sl_wisun_evt_t::connection_lost

SL_WISUN_MSG_CONNECTION_LOST_IND_ID event data


dhcp_vendor_data#

sl_wisun_msg_dhcp_vendor_data_ind_body_t sl_wisun_evt_t::dhcp_vendor_data

SL_WISUN_MSG_DHCP_VENDOR_DATA_IND_ID event data


direct_connect_link_available#

sl_wisun_msg_direct_connect_link_available_ind_body_t sl_wisun_evt_t::direct_connect_link_available

SL_WISUN_MSG_DIRECT_CONNECT_LINK_AVAILABLE_IND_ID event data


direct_connect_link_status#

sl_wisun_msg_direct_connect_link_status_ind_body_t sl_wisun_evt_t::direct_connect_link_status

SL_WISUN_MSG_DIRECT_CONNECT_LINK_STATUS_IND_ID event data


disconnected#

sl_wisun_msg_disconnected_ind_body_t sl_wisun_evt_t::disconnected

SL_WISUN_MSG_DISCONNECTED_IND_ID event data


error#

sl_wisun_msg_error_ind_body_t sl_wisun_evt_t::error

SL_WISUN_MSG_ERROR_IND_ID event data


evt#

union sl_wisun_evt_t::@0 sl_wisun_evt_t::evt

Event-specific data.

This structure contains the event-specific data.


header#

sl_wisun_msg_header_t sl_wisun_evt_t::header

Common event header.

This structure contains common information for all events. ID of the event is stored in the sl_wisun_msg_header_t.id field and is one of the values of sl_wisun_msg_ind_id_t. The other fields can be ignored.


join_state#

sl_wisun_msg_join_state_ind_body_t sl_wisun_evt_t::join_state

SL_WISUN_MSG_JOIN_STATE_IND_ID event data


lfn_multicast_reg#

sl_wisun_msg_lfn_multicast_reg_ind_body_t sl_wisun_evt_t::lfn_multicast_reg

SL_WISUN_MSG_LFN_MULTICAST_REG_IND_ID event data


lfn_wake_up#

sl_wisun_msg_lfn_wake_up_ind_body_t sl_wisun_evt_t::lfn_wake_up

SL_WISUN_MSG_LFN_WAKE_UP_IND_ID event data


logger_event#

sl_wisun_msg_logger_event_ind_body_t sl_wisun_evt_t::logger_event

SL_WISUN_MSG_LOGGER_EVENT_IND_ID event data


mode_switch_fallback#

sl_wisun_msg_mode_switch_fallback_ind_body_t sl_wisun_evt_t::mode_switch_fallback

SL_WISUN_MSG_MODE_SWITCH_FALLBACK_IND_ID event data


network_update#

sl_wisun_msg_network_update_ind_body_t sl_wisun_evt_t::network_update

SL_WISUN_MSG_NETWORK_UPDATE_IND_ID event data


pan_defect#

sl_wisun_msg_pan_defect_ind_body_t sl_wisun_evt_t::pan_defect

SL_WISUN_MSG_PAN_DEFECT_IND_ID event data


regulation_tx_level#

sl_wisun_msg_regulation_tx_level_ind_body_t sl_wisun_evt_t::regulation_tx_level

SL_WISUN_MSG_REGULATION_TX_LEVEL_IND_ID event data


rx_frame#

sl_wisun_msg_rx_frame_ind_body_t sl_wisun_evt_t::rx_frame

SL_WISUN_MSG_RX_FRAME_IND_ID event data


socket_closing#

sl_wisun_msg_socket_closing_ind_body_t sl_wisun_evt_t::socket_closing

SL_WISUN_MSG_SOCKET_CLOSING_IND_ID event data


socket_connected#

sl_wisun_msg_socket_connected_ind_body_t sl_wisun_evt_t::socket_connected

SL_WISUN_MSG_SOCKET_CONNECTED_IND_ID event data


socket_connection_available#

sl_wisun_msg_socket_connection_available_ind_body_t sl_wisun_evt_t::socket_connection_available

SL_WISUN_MSG_SOCKET_CONNECTION_AVAILABLE_IND_ID event data


socket_data#

sl_wisun_msg_socket_data_ind_body_t sl_wisun_evt_t::socket_data

SL_WISUN_MSG_SOCKET_DATA_IND_ID event data


socket_data_available#

sl_wisun_msg_socket_data_available_ind_body_t sl_wisun_evt_t::socket_data_available

SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID event data


socket_data_sent#

sl_wisun_msg_socket_data_sent_ind_body_t sl_wisun_evt_t::socket_data_sent

SL_WISUN_MSG_SOCKET_DATA_SENT_IND_ID event data