Request message body.

Public Attributes#

IP address of the remote peer.

uint16_t

Port number of the remote peer.

uint16_t

Reserved, set to zero.

int32_t

ID of the socket.

Public Attribute Documentation#

remote_address#

in6_addr_t sl_wisun_msg_connect_socket_req_body_t::remote_address

IP address of the remote peer.


remote_port#

uint16_t sl_wisun_msg_connect_socket_req_body_t::remote_port

Port number of the remote peer.


reserved#

uint16_t sl_wisun_msg_connect_socket_req_body_t::reserved

Reserved, set to zero.


socket_id#

int32_t sl_wisun_msg_connect_socket_req_body_t::socket_id

ID of the socket.