You are viewing documentation for version:2.11.0PDFRequest message body. Public Attributes#uint8_tdataData to write. uint16_tdata_lengthAmount of data to write. uint16_treservedReserved, set to zero. int32_tsocket_idID of the socket. Public Attribute Documentation#data#uint8_t sl_wisun_msg_send_on_socket_req_body_t::data[]Data to write. data_length#uint16_t sl_wisun_msg_send_on_socket_req_body_t::data_lengthAmount of data to write. reserved#uint16_t sl_wisun_msg_send_on_socket_req_body_t::reservedReserved, set to zero. socket_id#int32_t sl_wisun_msg_send_on_socket_req_body_t::socket_idID of the socket.