You are viewing documentation for version:2.11.1PDFRequest message body. Public Attributes#uint16_tregistration_lifetime_mRegistration lifetime in minutes. uint16_treservedReserved, set to zero. in6_addr_ttarget_addressTarget Address. Public Attribute Documentation#registration_lifetime_m#uint16_t sl_wisun_msg_register_address_req_body_t::registration_lifetime_mRegistration lifetime in minutes. reserved#uint16_t sl_wisun_msg_register_address_req_body_t::reservedReserved, set to zero. target_address#in6_addr_t sl_wisun_msg_register_address_req_body_t::target_addressTarget Address.