You are viewing documentation for version:2.11.1PDFRequest message body. Public Attributes#uint8_tidentityEAP identity. uint8_tidentity_lengthLength of EAP identity. uint8_treservedReserved, set to zero. Public Attribute Documentation#identity#uint8_t sl_wisun_msg_set_eap_identity_req_body_t::identity[SL_WISUN_EAP_IDENTITY_SIZE]EAP identity. identity_length#uint8_t sl_wisun_msg_set_eap_identity_req_body_t::identity_lengthLength of EAP identity. reserved#uint8_t sl_wisun_msg_set_eap_identity_req_body_t::reserved[3]Reserved, set to zero.