You are viewing documentation for version:
Confirmation message body.
Public Attributes#
int16_t
Number of bytes received;.
Public Attribute Documentation#
data_length#
int16_t sl_wisun_msg_socket_recvmsg_cnf_body_t::data_length
Number of bytes received;.
error_code#
int32_t sl_wisun_msg_socket_recvmsg_cnf_body_t::error_code
code of the error
reserved#
uint16_t sl_wisun_msg_socket_recvmsg_cnf_body_t::reserved
reserved, set to zero
status#
uint32_t sl_wisun_msg_socket_recvmsg_cnf_body_t::status
Status of the request.