Indication message body.

Public Attributes#

uint64_t

Expected time to next wake-up in microseconds.

uint32_t

Status of the indication.

uint32_t

Expected wake-up duration in microseconds.

Public Attribute Documentation#

next_wup_us#

uint64_t sl_wisun_msg_lfn_wake_up_ind_body_t::next_wup_us

Expected time to next wake-up in microseconds.


Definition at line 520 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

status#

uint32_t sl_wisun_msg_lfn_wake_up_ind_body_t::status

Status of the indication.


Definition at line 516 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

wup_duration_us#

uint32_t sl_wisun_msg_lfn_wake_up_ind_body_t::wup_duration_us

Expected wake-up duration in microseconds.


Definition at line 518 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h