Indication message body.
Public Attribute Documentation#
flags#
uint32_t sl_wisun_msg_network_update_ind_body_t::flags
Bit mask indicating the changes.
bit SL_WISUN_NETWORK_UPDATE_FLAGS_GLOBAL_IP: Global IP address has changed
bit SL_WISUN_NETWORK_UPDATE_FLAGS_PRIMARY_PARENT: primary parent has changed
bit SL_WISUN_NETWORK_UPDATE_FLAGS_SECONDARY_PARENT: secondary parent has changed
Definition at line
124
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
status#
uint32_t sl_wisun_msg_network_update_ind_body_t::status
Status of the indication.
Definition at line
119
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h