MPL parameter set.
Public Attributes#
uint8_t
MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.
uint16_t
MPL seed set entry lifetime (seconds)
MPL trickle timer.
uint8_t
MPL trickle timer expirations.
Public Attribute Documentation#
seed_id_type#
uint8_t sl_wisun_params_mpl::seed_id_type
MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.
seed_set_entry_lifetime_s#
uint16_t sl_wisun_params_mpl::seed_set_entry_lifetime_s
MPL seed set entry lifetime (seconds)