Statistic ping type definition.
Public Attributes#
uint32_t
Average echo time millisecond.
uint16_t
Lost packet count.
uint32_t
Maximum echo time millisecond.
uint32_t
Minimum echo time millisecond.
uint16_t
Packet count.
uint16_t
Packet length.
Wi-SUN remote address.
Public Attribute Documentation#
avg_time_ms#
uint32_t sl_wisun_ping_stat::avg_time_ms
Average echo time millisecond.
Definition at line
143
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
lost#
uint16_t sl_wisun_ping_stat::lost
Lost packet count.
Definition at line
137
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
max_time_ms#
uint32_t sl_wisun_ping_stat::max_time_ms
Maximum echo time millisecond.
Definition at line
141
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
min_time_ms#
uint32_t sl_wisun_ping_stat::min_time_ms
Minimum echo time millisecond.
Definition at line
139
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
packet_count#
uint16_t sl_wisun_ping_stat::packet_count
Packet count.
Definition at line
133
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
packet_length#
uint16_t sl_wisun_ping_stat::packet_length
Packet length.
Definition at line
135
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
remote_addr#
sockaddr_in6_t sl_wisun_ping_stat::remote_addr
Wi-SUN remote address.
Definition at line
131
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h