You are viewing documentation for version:2.7.0Wisun setting structure. Public Attributes#uint8_tdevice_typeDevice type. boolis_default_phydefault flag uint8_tkeychainKey chain. uint8_tkeychain_indexKey chain index. uint8_tlfn_profileLFN profile. charnetwork_nameNetwork Name. uint8_tnetwork_sizeNetwork size. sl_wisun_phy_config_tphyPHY settings. int16_ttx_power_ddbmTX Power. Public Attribute Documentation#device_type#uint8_t app_setting_wisun::device_typeDevice type. is_default_phy#bool app_setting_wisun::is_default_phydefault flag keychain#uint8_t app_setting_wisun::keychainKey chain. keychain_index#uint8_t app_setting_wisun::keychain_indexKey chain index. lfn_profile#uint8_t app_setting_wisun::lfn_profileLFN profile. network_name#char app_setting_wisun::network_name[APP_SETTING_NETWORK_NAME_MAX_SIZE]Network Name. network_size#uint8_t app_setting_wisun::network_sizeNetwork size. phy#sl_wisun_phy_config_t app_setting_wisun::phyPHY settings. tx_power_ddbm#int16_t app_setting_wisun::tx_power_ddbmTX Power.