You are viewing documentation for version:2.7.0Indication message body. Public Attributes#in6_addr_tlink_local_ipv6LinkLocal IPv6 address of the client. uint32_tlink_statusLink status. Public Attribute Documentation#link_local_ipv6#in6_addr_t sl_wisun_msg_direct_connect_link_status_ind_body_t::link_local_ipv6LinkLocal IPv6 address of the client. link_status#uint32_t sl_wisun_msg_direct_connect_link_status_ind_body_t::link_statusLink status.