You are viewing documentation for version:2.7.0Indication message body. Public Attributes#uint8_tframeReceived frame. uint16_tlengthFrame length in bytes. uint32_tstatusStatus of the indication. uint64_ttimestamp_usTimestamp in microseconds. Public Attribute Documentation#frame#uint8_t sl_wisun_msg_rx_frame_ind_body_t::frame[]Received frame. length#uint16_t sl_wisun_msg_rx_frame_ind_body_t::lengthFrame length in bytes. status#uint32_t sl_wisun_msg_rx_frame_ind_body_t::statusStatus of the indication. timestamp_us#uint64_t sl_wisun_msg_rx_frame_ind_body_t::timestamp_usTimestamp in microseconds.