Wi-SUN Stack API#

Wi-SUN Stack API is based on requests from the application to the stack and events from the stack to the application.

Requests are made using function calls, where a function call either performs the required action immediately or initiates an internal operation within the stack, which terminates with an event. All events contain a status code, indicating the result of the requested operation. Events are also used by the stack to notify the application of any important information, such as the state of the connection.

The application is expected to override sl_wisun_on_event() to handle events from the stack. Because all events share a common header, the function may be implemented as a switch statement. The event-specific data can be accessed through the sl_wisun_evt_t::evt union.

void sl_wisun_on_event(sl_wisun_evt_t *evt)
{
  switch (evt->header.id) {
    case SL_WISUN_MSG_CONNECTED_IND_ID:
      handle_connected_event(evt->evt.connected);
      break;
    default:
      break;
  }
}

The API is thread-safe, which means can be called from multiple RTOS tasks. The stack guarantees that only a single request is executed at a time and that requests are handled in the order they were made. Event callback is executed in a different context than the request, so the API functions may be called from the event callback.

Modules#

Wi-SUN API events

Wi-SUN API type definitions

Wi-SUN API availability

Wi-SUN Regional Regulation API

Border Router API

Socket API

Select API

Callbacks#

void
sl_wisun_on_event(sl_wisun_evt_t *evt)

Callback handler for a single event.

Functions#

sl_status_t
sl_wisun_accept_direct_connect_link(in6_addr_t *link_local_ipv6)

Accept a Direct Connect link.

sl_status_t
sl_wisun_allow_mac_address(const sl_wisun_mac_address_t *address)

Add a MAC address to the list of allowed addresses.

sl_status_t

Clear the credential cache.

sl_status_t
sl_wisun_config_concurrent_detection(bool enable_tx, uint8_t reserved)

Configure concurrent detection.

sl_status_t
sl_wisun_config_mode_switch(uint8_t mode, uint8_t phy_mode_id, const sl_wisun_mac_address_t *neighbor_address, bool reserved)

Set the mode switch configuration.

sl_status_t
sl_wisun_config_neighbor_table(uint8_t max_child_count, uint8_t max_neighbor_count, uint16_t max_security_neighbor_count)

Configure neighbor table size.

sl_status_t
sl_wisun_deny_mac_address(const sl_wisun_mac_address_t *address)

Add a MAC address to the list of denied addresses.

sl_status_t

Disconnect from the Wi-SUN network.

sl_status_t
sl_wisun_get_excluded_channel_mask(sl_wisun_channel_mask_type_t type, sl_wisun_channel_mask_t *channel_mask, uint32_t *channel_count)

Get the mask of channels excluded from channel plan.

sl_status_t
sl_wisun_get_ip_address(sl_wisun_ip_address_type_t address_type, in6_addr_t *address)

Read an IP address.

sl_status_t
sl_wisun_get_join_state(sl_wisun_join_state_t *join_state)

Get the current join state.

sl_status_t
sl_wisun_get_mac_address(sl_wisun_mac_address_t *address)

Get the current device MAC address in use.

sl_status_t
sl_wisun_get_neighbor_count(uint8_t *neighbor_count)

Get the number of RPL neighbors (parents and children).

sl_status_t
sl_wisun_get_neighbor_info(const sl_wisun_mac_address_t *neighbor_mac_address, sl_wisun_neighbor_info_t *neighbor_info)

Get information about a RPL neighbor (parent or child).

sl_status_t
sl_wisun_get_neighbors(uint8_t *neighbor_count, sl_wisun_mac_address_t *neighbor_mac_addresses)

Get a list of RPL neighbor (parents and children) MAC addresses.

sl_status_t
sl_wisun_get_network_info(sl_wisun_network_info_t *network_info)

Get Wi-SUN network information.

sl_status_t
sl_wisun_get_pom_ie(uint8_t *phy_mode_id_count, uint8_t *phy_mode_ids, uint8_t *is_mdr_command_capable)

Get the POM-IE configuration.

sl_status_t
sl_wisun_get_rpl_info(sl_wisun_rpl_info_t *rpl_info)

Get RPL information.

sl_status_t
sl_wisun_get_stack_version(uint8_t *major, uint8_t *minor, uint8_t *patch, uint16_t *build)

Get the Wi-SUN stack version.

sl_status_t
sl_wisun_get_statistics(sl_wisun_statistics_type_t statistics_type, sl_wisun_statistics_t *statistics)

Read a set of statistics.

sl_status_t
sl_wisun_join(const uint8_t *name, sl_wisun_phy_config_t *phy_config)

Initiate a connection to a Wi-SUN network.

sl_status_t

Reset all the the past hour transmissions counters.

sl_status_t
sl_wisun_reset_statistics(sl_wisun_statistics_type_t statistics_type)

Reset a set of statistics in the stack.

sl_status_t
sl_wisun_set_advert_fragment_duration(uint32_t fragment_duration_ms)

Set the async transmission fragmentation parameters.

sl_status_t
sl_wisun_set_allowed_channel_mask(const sl_wisun_channel_mask_t *channel_mask)

Set a mask of operating channels.

sl_status_t
sl_wisun_set_channel_mask(const sl_wisun_channel_mask_t *channel_mask)

Set a mask of operating channels.

sl_status_t
sl_wisun_set_connection_parameters(const sl_wisun_connection_params_t *params)

Configure the FFN parameter set.

sl_status_t
sl_wisun_set_device_certificate(uint16_t certificate_options, uint16_t certificate_length, const uint8_t *certificate)

Set the device certificate used to authenticate to the authentication server.

sl_status_t
sl_wisun_set_device_private_key(uint16_t key_options, uint16_t key_length, const uint8_t *key)

Set the device private key used to authenticate to the authentication server.

sl_status_t

Set the device private key used to authenticate to the authentication server.

sl_status_t
sl_wisun_set_device_type(sl_wisun_device_type_t device_type)

Set the device type.

sl_status_t
sl_wisun_set_direct_connect_pmk(const uint32_t pmk_key_id)

Set the Pairwise Master Key (PMK) to use for Direct Connect.

sl_status_t

Enable/disable Direct Connect.

sl_status_t
sl_wisun_set_eap_identity(uint8_t identity_length, const uint8_t *identity)

Set EAP identity for authentication.

sl_status_t
sl_wisun_set_event_filter(const sl_wisun_mac_address_t *address, uint64_t events)

Set Filter for network events.

sl_status_t
sl_wisun_set_leaf(bool is_leaf)

Set the RPL leaf mode.

sl_status_t
sl_wisun_set_lfn_parameters(const sl_wisun_lfn_params_t *params)

Configure the LFN parameter set.

sl_status_t
sl_wisun_set_lfn_support(uint8_t lfn_limit)

Configure LFN parenting support.

sl_status_t
sl_wisun_set_mac_address(const sl_wisun_mac_address_t *address)

Set the device MAC address to be used.

sl_status_t
sl_wisun_set_mode_switch(uint8_t mode, uint8_t phy_mode_id, const sl_wisun_mac_address_t *neighbor_address)

Set the PHY mode switch configuration.

sl_status_t
sl_wisun_set_neighbor_table_size(uint8_t size) SL_DEPRECATED_API_SDK_2025_6

Set neighbor table size.

sl_status_t
sl_wisun_set_phy_sensitivity(uint8_t phy_mode_id, int16_t sensitivity_dbm)

Set the radio sensitivity for the given PHY.

sl_status_t
sl_wisun_set_pom_ie(uint8_t phy_mode_id_count, uint8_t phy_mode_ids[SL_WISUN_MAX_PHY_MODE_ID_COUNT], uint8_t is_mdr_command_capable)

Set the POM-IE configuration.

sl_status_t

Set the preferred PAN for this device.

sl_status_t
sl_wisun_set_pti_state(bool pti_state)

Set the PTI state.

sl_status_t
sl_wisun_set_regulation(sl_wisun_regulation_t regulation)

Set the regional regulation.

sl_status_t
sl_wisun_set_regulation_parameters(const sl_wisun_regulation_params_t *params)

Configure the regional regulation parameter set.

sl_status_t
sl_wisun_set_regulation_tx_thresholds(int8_t warning_threshold, int8_t alert_threshold)

Set the thresholds for transmission duration level event.

sl_status_t
sl_wisun_set_security_state(uint32_t security_state)

Set the connection security state.

sl_status_t
sl_wisun_set_trusted_certificate(uint16_t certificate_options, uint16_t certificate_length, const uint8_t *certificate)

Set a trusted CA certificate used to validate the authentication server certificate.

sl_status_t
sl_wisun_set_tx_power(int8_t tx_power) SL_DEPRECATED_API_SDK_2024_6

Set the maximum TX power.

sl_status_t
sl_wisun_set_tx_power_ddbm(int16_t tx_power_ddbm)

Set the maximum TX power.

sl_status_t
sl_wisun_set_unicast_settings(uint8_t dwell_interval_ms)

Set unicast settings.

sl_status_t
sl_wisun_trigger_frame(sl_wisun_frame_type_t frame_type)

Trigger a transmission of a periodic frame (FAN Discovery, RPL).

Callbacks Documentation#

sl_wisun_on_event#

void sl_wisun_on_event (sl_wisun_evt_t * evt)

Callback handler for a single event.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_evt_t *[out]evt

The event to be handled

This function is called when the stack sends an event to the application. The application can declare its own version this function to customize event handling. The default implementation discards all events.

See Also


Function Documentation#

sl_wisun_accept_direct_connect_link#

sl_status_t sl_wisun_accept_direct_connect_link (in6_addr_t * link_local_ipv6)

Accept a Direct Connect link.

Parameters
TypeDirectionArgument NameDescription
in6_addr_t *[in]link_local_ipv6

Link-Local IPv6 address of the client

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN (see Wi-SUN API availability)


sl_wisun_allow_mac_address#

sl_status_t sl_wisun_allow_mac_address (const sl_wisun_mac_address_t * address)

Add a MAC address to the list of allowed addresses.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]address

MAC address

  • sl_wisun_broadcast_mac: allow all MAC addresses

  • unicast address: allow the given MAC address

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function adds a MAC address to the list of allowed addresses. When the first address is added to the list, the list of denied addresses is cleared and the device will start preventing communication with any device whose MAC address does not match any of addresses on the list. By default, all MAC addresses are allowed. Up to 10 MAC addresses may be added to the list. The access list affects only directly connected nodes such as parents, children, and neighbors.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_clear_credential_cache#

sl_status_t sl_wisun_clear_credential_cache ()

Clear the credential cache.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function clears the cached authentication credentials stored in non-volatile storage. The function is intended for test purposes. Note that clearing the credential cache may prevent the node from reconnecting to the same parent until the corresponding cache entry has expired on the parent.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_config_concurrent_detection#

sl_status_t sl_wisun_config_concurrent_detection (bool enable_tx, uint8_t reserved)

Configure concurrent detection.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable_tx

TX state

  • true: TX is allowed with an alternate PHY

  • false: TX is not allowed with an alternate PHY

uint8_t[in]reserved

Reserved for future use, set to zero.

Returns

  • SL_STATUS_OK if the operation is successful, an error code otherwise.

This function configures whether an alternate PHY can be used concurrently with the base PHY. The alternate PHY must be enabled in the radio configuration to utilize this feature. When enabled, the alternate PHY is always accepted on receive. When TX state is set to true, the node will transmit to nodes that support the feature using the alternate PHY, instead of using the standard mode switch. TX is disabled by default.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_config_mode_switch#

sl_status_t sl_wisun_config_mode_switch (uint8_t mode, uint8_t phy_mode_id, const sl_wisun_mac_address_t * neighbor_address, bool reserved)

Set the mode switch configuration.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]mode

Mode switch configuration of the neighbor. If set to SL_WISUN_MODE_SWITCH_DEFAULT, the configuration of the neighbor is reset back to the default mode switch behavior.

uint8_t[in]phy_mode_id

PhyModeId to use when mode is set to SL_WISUN_MODE_SWITCH_ENABLED, ignored otherwise.

const sl_wisun_mac_address_t *[in]neighbor_address

MAC address of the neighbor to configure. If set to sl_wisun_broadcast_mac, configures the default mode switch behavior for all non-configured neighbors.

bool[in]reserved

Reserved for future use, set to false.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_config_neighbor_table#

sl_status_t sl_wisun_config_neighbor_table (uint8_t max_child_count, uint8_t max_neighbor_count, uint16_t max_security_neighbor_count)

Configure neighbor table size.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]max_child_count

Maximum number of RPL children Increasing this parameter means a higher number of potential neighbors while lowering it means reduced RAM consumption. The default value is 22.

uint8_t[in]max_neighbor_count

Maximum number of neighbors including children, parent, and temporary neighbors The default value is 32

uint16_t[in]max_security_neighbor_count

Maximum number of neigbors in the security table. Entries in the security table are removed on key expirations. Default value is 300

Returns

  • SL_STATUS_OK if successful, an error code otherwise

max_neighbor_count must be greater than max_child_count. max_neighbor_count - max_child_count represents the available neighbors for RPL parents and temporary neighbors (neighbors not yet registered, parent candidate or neighbors sending multicast). max_security_neighbor_count must be greater or equal than max_neighbor_count Each entry in the neighbor table consumes about 450 bytes of RAM. Each entry in the security neighbor table consumes about 50 bytes of RAM. Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_deny_mac_address#

sl_status_t sl_wisun_deny_mac_address (const sl_wisun_mac_address_t * address)

Add a MAC address to the list of denied addresses.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]address

MAC address

  • sl_wisun_broadcast_mac: deny all MAC addresses

  • unicast address: deny the given MAC address

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function adds a MAC address to the list of denied addresses. When the first address is added to the list, the list of allowed addresses is cleared and the device will start preventing communication with any device whose MAC address matches any of the addresses on the list. By default, all MAC addresses are allowed. Up to 10 MAC addresses may be added to the list. The access list affects only directly connected nodes such as parents, children, and neighbors.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_disconnect#

sl_status_t sl_wisun_disconnect ()

Disconnect from the Wi-SUN network.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function disconnects an active connection or cancels an ongoing connection attempt.

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_get_excluded_channel_mask#

sl_status_t sl_wisun_get_excluded_channel_mask (sl_wisun_channel_mask_type_t type, sl_wisun_channel_mask_t * channel_mask, uint32_t * channel_count)

Get the mask of channels excluded from channel plan.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_channel_mask_type_t[in]type

Type of channel mask to retrieve

sl_wisun_channel_mask_t *[out]channel_mask

Pointer where channel mask is written

uint32_t *[out]channel_count

Number of channels in the mask

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_ip_address#

sl_status_t sl_wisun_get_ip_address (sl_wisun_ip_address_type_t address_type, in6_addr_t * address)

Read an IP address.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_ip_address_type_t[in]address_type

Type of the IP address to read

in6_addr_t *[out]address

IP address to read

Returns

  • SL_STATUS_OK if successful, an error code otherwise.

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_get_join_state#

sl_status_t sl_wisun_get_join_state (sl_wisun_join_state_t * join_state)

Get the current join state.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_join_state_t *[out]join_state

Join state

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function retrieves the current state of the connection process. The function can only be used once a connection has been initiated.

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_get_mac_address#

sl_status_t sl_wisun_get_mac_address (sl_wisun_mac_address_t * address)

Get the current device MAC address in use.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_mac_address_t *[out]address

MAC address

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_neighbor_count#

sl_status_t sl_wisun_get_neighbor_count (uint8_t * neighbor_count)

Get the number of RPL neighbors (parents and children).

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]neighbor_count

Number of neighbors

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_neighbor_info#

sl_status_t sl_wisun_get_neighbor_info (const sl_wisun_mac_address_t * neighbor_mac_address, sl_wisun_neighbor_info_t * neighbor_info)

Get information about a RPL neighbor (parent or child).

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]neighbor_mac_address

Pointer to neighbor MAC address

sl_wisun_neighbor_info_t *[out]neighbor_info

Pointer to where the read information is stored

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_neighbors#

sl_status_t sl_wisun_get_neighbors (uint8_t * neighbor_count, sl_wisun_mac_address_t * neighbor_mac_addresses)

Get a list of RPL neighbor (parents and children) MAC addresses.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[inout]neighbor_count

Maximum number of neighbors to read on input, number of neighbors read on output

sl_wisun_mac_address_t *[out]neighbor_mac_addresses

Pointer to memory where to store neighbor MAC addresses

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_network_info#

sl_status_t sl_wisun_get_network_info (sl_wisun_network_info_t * network_info)

Get Wi-SUN network information.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_network_info_t *[out]network_info

Pointer where network information is written

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_pom_ie#

sl_status_t sl_wisun_get_pom_ie (uint8_t * phy_mode_id_count, uint8_t * phy_mode_ids, uint8_t * is_mdr_command_capable)

Get the POM-IE configuration.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]phy_mode_id_count

Number of PhyModeId retrieved

uint8_t *[out]phy_mode_ids

List of phy_mode_id_count PhyModeId. Caller must allocate space for at least SL_WISUN_MAX_PHY_MODE_ID_COUNT entries.

uint8_t *[out]is_mdr_command_capable

Set to 1 if the device supports MAC mode switch, 0 otherwise

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function retrieves the PHY operating mode information advertised to neighboring nodes.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_rpl_info#

sl_status_t sl_wisun_get_rpl_info (sl_wisun_rpl_info_t * rpl_info)

Get RPL information.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_rpl_info_t *[out]rpl_info

Pointer where RPL information is written

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, BR (see Wi-SUN API availability)


sl_wisun_get_stack_version#

sl_status_t sl_wisun_get_stack_version (uint8_t * major, uint8_t * minor, uint8_t * patch, uint16_t * build)

Get the Wi-SUN stack version.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]major

Wi-SUN stack version major

uint8_t *[out]minor

Wi-SUN stack version minor

uint8_t *[out]patch

Wi-SUN stack version patch

uint16_t *[out]build

Build number, set to 0 in public versions

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_get_statistics#

sl_status_t sl_wisun_get_statistics (sl_wisun_statistics_type_t statistics_type, sl_wisun_statistics_t * statistics)

Read a set of statistics.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_statistics_type_t[in]statistics_type

Type of statistics to read

sl_wisun_statistics_t *[out]statistics

Set of statistics read

Returns

  • SL_STATUS_OK if successful, an error code otherwise.

This function reads a set of statistics from the stack. Statistics are cumulative and reset when a connection is initiated or by calling sl_wisun_reset_statistics().

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_join#

sl_status_t sl_wisun_join (const uint8_t * name, sl_wisun_phy_config_t * phy_config)

Initiate a connection to a Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]name

Name of the Wi-SUN network as a zero-terminated string

sl_wisun_phy_config_t *[in]phy_config

Pointer to PHY configuration

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function initiates connection to a Wi-SUN network. Completion of the request is indicated with a SL_WISUN_MSG_CONNECTED_IND_ID event.

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_reset_regulation_duty_cycle#

sl_status_t sl_wisun_reset_regulation_duty_cycle (void )

Reset all the the past hour transmissions counters.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_reset_statistics#

sl_status_t sl_wisun_reset_statistics (sl_wisun_statistics_type_t statistics_type)

Reset a set of statistics in the stack.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_statistics_type_t[in]statistics_type

Type of statistics to reset

Returns

  • SL_STATUS_OK if successful, an error code otherwise.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_advert_fragment_duration#

sl_status_t sl_wisun_set_advert_fragment_duration (uint32_t fragment_duration_ms)

Set the async transmission fragmentation parameters.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]fragment_duration_ms

Max duration of a fragment in ms (min 500 ms)

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Async transmissions, such as Wi-SUN PAN advertisement packets, are sent to every allowed operating channel and may therefore block broadcast and unicast traffic. This impact can be reduced by splitting the channel list into fragments based on the maximum transmission duration and by forcing a delay between the fragments, allowing other traffic to occur. This function sets the maximum duration of a PA, PAS, PC, and PCS advertisement period fragments. A small value trades off longer connection times for shorter latencies. Setting the duration to SL_WISUN_ADVERT_FRAGMENT_DISABLE disables async transmission fragmentation.

By default, the maximum fragment duration is set to 500 ms.

Available in libraries: Full, FFN, BR (see Wi-SUN API availability)


sl_wisun_set_allowed_channel_mask#

sl_status_t sl_wisun_set_allowed_channel_mask (const sl_wisun_channel_mask_t * channel_mask)

Set a mask of operating channels.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_channel_mask_t *[in]channel_mask

Mask of operating channels

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets a mask of channels the device is allowed to operate in for unicast frequency hopping. By default, all channels in the channel plan are allowed. The mask can only be used to further restrict the channels. Channels outside the channel plan or channels internally excluded are ignored. This mask will be used in the following connections.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Warnings

  • By comparison to the Wi-SUN FAN specification, the channel mask logic is inverted. The specification references a mask of excluded channels.


sl_wisun_set_channel_mask#

sl_status_t sl_wisun_set_channel_mask (const sl_wisun_channel_mask_t * channel_mask)

Set a mask of operating channels.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_channel_mask_t *[in]channel_mask

Mask of operating channels

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets a mask of channels the device is allowed to operate in for unicast frequency hopping. By default, all channels in the channel plan are allowed. The mask can only be used to further restrict the channels. Channels outside the channel plan or channels internally excluded are ignored. This mask will be used in the following connections.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_connection_parameters#

sl_status_t sl_wisun_set_connection_parameters (const sl_wisun_connection_params_t * params)

Configure the FFN parameter set.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_connection_params_t *[in]params

Parameter set to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the FFN parameter set. These parameters impact connection time, bandwidth usage, and latency. Use of a predefined parameter set is recommended (Predefined FFN parameter sets). Small profile will be used by default for all missing configurations. The function must be called before initiating a connection.

Available in libraries: Full, FFN (see Wi-SUN API availability)


sl_wisun_set_device_certificate#

sl_status_t sl_wisun_set_device_certificate (uint16_t certificate_options, uint16_t certificate_length, const uint8_t * certificate)

Set the device certificate used to authenticate to the authentication server.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]certificate_options

Options for the certificate.

uint16_t[in]certificate_length

Size of the certificate data

const uint8_t *[in]certificate

Pointer to the certificate data

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the device certificate used during the authentication process. The corresponding device private key must be set using sl_wisun_set_device_private_key() or sl_wisun_set_device_private_key_id(). The supported certificate formats depend on application's Mbed TLS configuration. The default configuration supports PEM and DER formats.

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_set_device_private_key#

sl_status_t sl_wisun_set_device_private_key (uint16_t key_options, uint16_t key_length, const uint8_t * key)

Set the device private key used to authenticate to the authentication server.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]key_options

Options for the private key

uint16_t[in]key_length

Size of the private key data

const uint8_t *[in]key

Pointer to the private key data

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the device private key used during the authentication process. The corresponding device certificate must be set using sl_wisun_set_device_certificate(). The supported key formats depend on application's Mbed TLS configuration. The default configuration supports unencrypted PKCS#8 and SEC1 keys in PEM and DER formats.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_device_private_key_id#

sl_status_t sl_wisun_set_device_private_key_id (uint32_t key_id)

Set the device private key used to authenticate to the authentication server.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]key_id

Key ID of the private key

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the device private key using a key identifier, referencing a key stored in PSA cryptography module. The corresponding device certificate must be set using sl_wisun_set_device_certificate(). The stored key must have correct PSA key attributes, see the Wi-SUN FAN Security Concepts and Design Considerations document for details.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_device_type#

sl_status_t sl_wisun_set_device_type (sl_wisun_device_type_t device_type)

Set the device type.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_device_type_t[in]device_type

Type of the device

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the operational mode of the node.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Note

  • This is a no-op with BR, FFN and LFN libraries.


sl_wisun_set_direct_connect_pmk#

sl_status_t sl_wisun_set_direct_connect_pmk (const uint32_t pmk_key_id)

Set the Pairwise Master Key (PMK) to use for Direct Connect.

Parameters
TypeDirectionArgument NameDescription
const uint32_t[in]pmk_key_id

The Pairwise Master Key (PMK) ID to use.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the Direct Connect PMK using a key identifier, referencing a key stored in PSA cryptography module. The stored key must have correct PSA key attributes, see the Wi-SUN FAN Security Concepts and Design Considerations document for details.

Available in libraries: Full, FFN (see Wi-SUN API availability)


sl_wisun_set_direct_connect_state#

sl_status_t sl_wisun_set_direct_connect_state (bool is_enabled)

Enable/disable Direct Connect.

Parameters
TypeDirectionArgument NameDescription
bool[in]is_enabled

Direct Connect status

  • true: Direct Connect is enabled

  • false: Direct Connect is disabled

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN (see Wi-SUN API availability)

Note

  • Enabling this feature may increase connection time.


sl_wisun_set_eap_identity#

sl_status_t sl_wisun_set_eap_identity (uint8_t identity_length, const uint8_t * identity)

Set EAP identity for authentication.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]identity_length

Length of EAP identity in bytes

const uint8_t *[in]identity

EAP identity to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the identity used in the EAP Identity Response during EAP authentication. The function must be called before initiating a connection. No checks are performed on the identity, the caller is responsible for formatting it correctly. In particular, RFC3748 requires that the identity must not be NULL terminated. If not set, the identity defaults to "Anonymous".

Available in libraries: Full, FFN, LFN (see Wi-SUN API availability)


sl_wisun_set_event_filter#

sl_status_t sl_wisun_set_event_filter (const sl_wisun_mac_address_t * address, uint64_t events)

Set Filter for network events.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]address

MAC address to filter events

  • unicast address: set the filter for the given MAC address

  • sl_wisun_broadcast_mac: set the filter for all MAC addresses

uint64_t[in]events

Bitmask of accepted events.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function configures a filter for network events based on the specified MAC address and a bitmask of sl_wisun_event_type_t that defines the filtered events. The events are delivered through Silicon Labs’ Event System API1. To receive them, user must call sl_event_subscribe with SL_EVENT_CLASS_WISUN. To disable a filter, set the events bitmask to 0. This function can be called at any time.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_leaf#

sl_status_t sl_wisun_set_leaf (bool is_leaf)

Set the RPL leaf mode.

Parameters
TypeDirectionArgument NameDescription
bool[in]is_leaf

RPL leaf mode

  • true: RPL leaf mode is enabled

  • false: RPL leaf mode is disabled

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function configures RPL leaf mode on FFNs. When enabled, it prevents the FFN from parenting other nodes (FFN or LFN).

Available in libraries: Full, FFN (see Wi-SUN API availability)


sl_wisun_set_lfn_parameters#

sl_status_t sl_wisun_set_lfn_parameters (const sl_wisun_lfn_params_t * params)

Configure the LFN parameter set.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_lfn_params_t *[in]params

Parameter set to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the LFN parameter set. These parameters impact connection time, bandwidth usage, power consumption, and latency. Use of a predefined parameter set is recommended (Predefined LFN parameter sets). Test profile will be used by default for all missing configurations. The function must be called before initiating a connection.

Available in libraries: Full, LFN (see Wi-SUN API availability)


sl_wisun_set_lfn_support#

sl_status_t sl_wisun_set_lfn_support (uint8_t lfn_limit)

Configure LFN parenting support.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]lfn_limit

Maximum number of LFN children

  • 0: LFN parenting is disabled in the node

  • **> 0**: Maximum number of LFN children the node can parent

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the maximum number of LFN children this node can parent. Set sl_wisun_config_neighbor_table accordingly.

Available in libraries: Full, FFN (see Wi-SUN API availability)


sl_wisun_set_mac_address#

sl_status_t sl_wisun_set_mac_address (const sl_wisun_mac_address_t * address)

Set the device MAC address to be used.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_mac_address_t *[in]address

MAC address

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the MAC address for use in the following connections. By default, the device will use the built-in unique device MAC address. The address is reset to the built-in value upon power up.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_mode_switch#

sl_status_t sl_wisun_set_mode_switch (uint8_t mode, uint8_t phy_mode_id, const sl_wisun_mac_address_t * neighbor_address)

Set the PHY mode switch configuration.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]mode

Mode switch configuration of the neighbor. If set to SL_WISUN_MODE_SWITCH_DEFAULT, the configuration of the neighbor is reset back to the default mode switch behavior.

uint8_t[in]phy_mode_id

PhyModeId to use when mode is set to SL_WISUN_MODE_SWITCH_ENABLED, ignored otherwise.

const sl_wisun_mac_address_t *[in]neighbor_address

MAC address of the neighbor to configure. If set to sl_wisun_broadcast_mac, configures the default mode switch behavior for all non-configured neighbors.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_neighbor_table_size#

sl_status_t sl_wisun_set_neighbor_table_size (uint8_t size)

Set neighbor table size.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]size

Size of the neighbor table

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the limit of regular neighbors supported by the node [1, 245], without considering temporary or RPL parents. Increasing this parameter means a higher number of potential neighbors while lowering it means reduced RAM consumption. The default value is 22.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

DeprecatedThis function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_config_neighbor_table() instead.


sl_wisun_set_phy_sensitivity#

sl_status_t sl_wisun_set_phy_sensitivity (uint8_t phy_mode_id, int16_t sensitivity_dbm)

Set the radio sensitivity for the given PHY.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]phy_mode_id

PHY mode ID

int16_t[in]sensitivity_dbm

Sensitivity in dBm

Returns

  • SL_STATUS_OK if successful, SL_STATUS_INVALID_PARAMETER if the PHY mode ID is invalid, SL_STATUS_FULL if you a have already set SL_WISUN_MAX_PHY_MODE_ID_COUNT different entries

This function sets the radio sensitivity for RX state. It allows to fine tune it according to the user's hardware and needs. The stack possesses a set of default values for each PHY mode, but the user can override them with this function. User's modifications generated by this API are not saved in the NVM.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Warnings

  • Changing the RX sensitivity can have a significant impact on the network's behavior and performance and should be done with caution. The stack follows the Wi-SUN specification, and as such, takes a margin around the given sensitivity (hysteresis). It is strongly advised to only use this API when using a Low-noise amplifier with an FEM.


sl_wisun_set_pom_ie#

sl_status_t sl_wisun_set_pom_ie (uint8_t phy_mode_id_count, uint8_t phy_mode_ids, uint8_t is_mdr_command_capable)

Set the POM-IE configuration.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]phy_mode_id_count

Number of PhyModeId to configure

uint8_t[in]phy_mode_ids

List of phy_mode_id_count PhyModeId. It must not contain the base operating mode.

uint8_t[in]is_mdr_command_capable

Indicate if the device supports MAC mode switch. Feature currently unsupported, must be set to 0.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the PHY operating mode information advertised to neighboring nodes. By default the PhyModeId list contains the first fifteen PhyModeId listed in radio multi-PHY configuration, MAC mode switch is disabled.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_preferred_pan#

sl_status_t sl_wisun_set_preferred_pan (uint16_t pan_id)

Set the preferred PAN for this device.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]pan_id

Preferred PAN ID. Set to 0xFFFF to disable.

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets a preferred PAN ID that the device will always select during connection if available, or seek to roam to while connected to another PAN.

Note


sl_wisun_set_pti_state#

sl_status_t sl_wisun_set_pti_state (bool pti_state)

Set the PTI state.

Parameters
TypeDirectionArgument NameDescription
bool[in]pti_state

PTI state

  • true: PTI is enabled

  • false: PTI is disabled

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets Packet Trace Interface (PTI) state. PTI is enabled by default.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_regulation#

sl_status_t sl_wisun_set_regulation (sl_wisun_regulation_t regulation)

Set the regional regulation.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_regulation_t[in]regulation

Regional regulation

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function applies the appropriate parameter set from Predefined regional regulation parameter sets to be used for upcoming connections. The selected regional regulation will impact both the Wi-SUN stack performance and its behavior. See regulation standards for details. No regulation is set by default.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Note


sl_wisun_set_regulation_parameters#

sl_status_t sl_wisun_set_regulation_parameters (const sl_wisun_regulation_params_t * params)

Configure the regional regulation parameter set.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_regulation_params_t *[in]params

Parameter set to use

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_regulation_tx_thresholds#

sl_status_t sl_wisun_set_regulation_tx_thresholds (int8_t warning_threshold, int8_t alert_threshold)

Set the thresholds for transmission duration level event.

Parameters
TypeDirectionArgument NameDescription
int8_t[in]warning_threshold

Warning threshold in percent or -1 to disable

int8_t[in]alert_threshold

Alert threshold in percent or -1 to disable

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the thresholds for transmission duration level event. When set and when a regional regulation is enabled using sl_wisun_set_regulation(), a SL_WISUN_MSG_REGULATION_TX_LEVEL_IND_ID event is sent when one of the configured thresholds is exceeded. This can be used by the application to prevent exceeding the total transmission duration allowed in the regional regulation. Thresholds are defined as a percentage of the maximum transmission duration permitted by the regional regulation.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_security_state#

sl_status_t sl_wisun_set_security_state (uint32_t security_state)

Set the connection security state.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]security_state

Connection security state

  • 0: Authentication and link encryption are disabled

  • 1: Authentication and link encryption are enabled

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the connection security state. By default, authentication and link encryption are enabled. The function is intended for test purposes.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Note

  • Authentication and link encryption can only be disabled when the application is linked against a library supporting this option.


sl_wisun_set_trusted_certificate#

sl_status_t sl_wisun_set_trusted_certificate (uint16_t certificate_options, uint16_t certificate_length, const uint8_t * certificate)

Set a trusted CA certificate used to validate the authentication server certificate.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]certificate_options

Options for the certificate

uint16_t[in]certificate_length

Size of the certificate data

const uint8_t *[in]certificate

Pointer to the certificate data

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets a trusted CA certificate for validiting the authentication server certificate during the authentication process. The supported certificate formats depend on application's Mbed TLS configuration. The default configuration supports PEM and DER formats. When PEM is used, the certificate data may contain multiple concatenated certificates.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)


sl_wisun_set_tx_power#

sl_status_t sl_wisun_set_tx_power (int8_t tx_power)

Set the maximum TX power.

Parameters
TypeDirectionArgument NameDescription
int8_t[in]tx_power

TX power in dBm

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the maximum TX power. The device may use a lower value based on internal decision making or hardware limitations but will never exceed the given value. The function must be called before initiating a connection.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

DeprecatedThis function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_set_tx_power_ddbm() instead.


sl_wisun_set_tx_power_ddbm#

sl_status_t sl_wisun_set_tx_power_ddbm (int16_t tx_power_ddbm)

Set the maximum TX power.

Parameters
TypeDirectionArgument NameDescription
int16_t[in]tx_power_ddbm

TX power in deci-dBm

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the maximum TX power. The device may use a lower value based on internal decision making or hardware limitations but will never exceed the given value. The function must be called before initiating a connection.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)

Note

  • When replacing sl_wisun_set_tx_power() function calls with this function, note the change from dBm units to deci-dBm units.


sl_wisun_set_unicast_settings#

sl_status_t sl_wisun_set_unicast_settings (uint8_t dwell_interval_ms)

Set unicast settings.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]dwell_interval_ms

Unicast Dwell Interval (15-255 ms)

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function sets the parameters for unicast channel hopping to be used in the following connections. The Unicast Dwell Interval specifies the duration which the node will listen to a channel within its listening schedule. The default value is 255 ms.

Available in libraries: Full, FFN, BR (see Wi-SUN API availability)


sl_wisun_trigger_frame#

sl_status_t sl_wisun_trigger_frame (sl_wisun_frame_type_t frame_type)

Trigger a transmission of a periodic frame (FAN Discovery, RPL).

Parameters
TypeDirectionArgument NameDescription
sl_wisun_frame_type_t[in]frame_type

Type of frame to transmit

Returns

  • SL_STATUS_OK if successful, an error code otherwise

This function causes a periodic frame (FAN Discovery, RPL) to be transmitted immediately. The frame can only be transmitted in the appropriate connection state, i.e. the associated trickle timer must be running. The function is intended for test purposes.

Available in libraries: Full, FFN, LFN, BR (see Wi-SUN API availability)