Public Attributes#
char const *const
Human readable name.
char const *const
Human readable info.
Minimum value.
Maximum value.
Size of the parameter in bytes.
Type of the parameter, e.g.: signed, unsigned.
Default data.
const struct _cc_config_parameter_attributes_t::@0
Public Attribute Documentation#
name#
char const* const _cc_config_parameter_attributes_t::name
Human readable name.
Definition at line
79
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
info#
char const* const _cc_config_parameter_attributes_t::info
Human readable info.
Definition at line
80
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
min_value#
const cc_config_parameter_value_t _cc_config_parameter_attributes_t::min_value
Minimum value.
Definition at line
81
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
max_value#
const cc_config_parameter_value_t _cc_config_parameter_attributes_t::max_value
Maximum value.
Definition at line
82
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
size#
cc_config_parameter_size_t _cc_config_parameter_attributes_t::size
Size of the parameter in bytes.
Definition at line
83
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
format#
const cc_config_parameter_format_t _cc_config_parameter_attributes_t::format
Type of the parameter, e.g.: signed, unsigned.
Definition at line
84
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
default_value#
const cc_config_parameter_value_t _cc_config_parameter_attributes_t::default_value
Default data.
Definition at line
85
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
flags#
const struct _cc_config_parameter_attributes_t::@0 _cc_config_parameter_attributes_t::flags
Definition at line
90
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h