Struct used to pass operational data to TSE module.

Public Attributes#

uint8_t
uint8_t *

index of notification in notifications array

uint8_t

Pointer to event parameters.

Public Attribute Documentation#

rxOptions#

RECEIVE_OPTIONS_TYPE_EX s_CC_notification_data_t_::rxOptions

rxOptions


Definition at line 67 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

index#

uint8_t s_CC_notification_data_t_::index

Definition at line 68 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

pEventParameters#

uint8_t* s_CC_notification_data_t_::pEventParameters

index of notification in notifications array


Definition at line 69 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

eventParamLength#

uint8_t s_CC_notification_data_t_::eventParamLength

Pointer to event parameters.


Definition at line 70 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h