MultilevelSwitch#

Modules#

cc_multilevel_switch_t

Enumerations#

enum
CCMLS_PRIMARY_SWITCH_UP
CCMLS_PRIMARY_SWITCH_DOWN
CCMLS_PRIMARY_SWITCH_RESERVED
CCMLS_PRIMARY_SWITCH_NO_UP_DOWN_MOTION
}

Enumeration for "Start Level Change" command.

enum
CCMLS_IGNORE_START_LEVEL_FALSE
CCMLS_IGNORE_START_LEVEL_TRUE
}

Enumeration for "Start Level Change" command.

enum
CCMLS_SECONDARY_SWITCH_INCREMENT
CCMLS_SECONDARY_SWITCH_DECREMENT
CCMLS_SECONDARY_SWITCH_RESERVED
CCMLS_SECONDARY_SWITCH_NO_INC_DEC
}

Enumeration for "Start Level Change" command.

Typedefs#

typedef void(*
cc_multilevel_switch_callback_t)(struct cc_multilevel_switch_t *p_switch)

Functions#

CmdClassMultilevelSwitchStartLevelChange(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, void(*pCbFunc)(TRANSMISSION_RESULT *pTransmissionResult), CCMLS_PRIMARY_SWITCH_T primarySwitch, CCMLS_IGNORE_START_LEVEL_T fIgnoreStartLevel, CCMLS_SECONDARY_SWITCH_T secondarySwitch, uint8_t primarySwitchStartLevel, uint8_t duration, uint8_t secondarySwitchStepSize)

Initiates the transmission of a "Multilevel Switch Start Level Change" command.

CmdClassMultilevelSwitchStopLevelChange(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, void(*pCbFunc)(TRANSMISSION_RESULT *pTransmissionResult))

Initiates the transmission of a "Multilevel Switch Stop Level Change" command.

CmdClassMultilevelSwitchSetTransmit(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, void(*pCbFunc)(TRANSMISSION_RESULT *pTransmissionResult), uint8_t value, uint8_t duration)

Initiates the transmission of a "Multilevel Switch Set" command.

void
cc_multilevel_switch_set(cc_multilevel_switch_t *p_switch, uint8_t value, uint8_t duration)

Sets the value of a given multilevel switch.

void
cc_multilevel_switch_start_level_change(cc_multilevel_switch_t *p_switch, bool up, bool ignore_start_level, uint8_t start_level, uint8_t duration)

Starts changing the value of a given multilevel switch.

void
cc_multilevel_switch_stop_level_change(cc_multilevel_switch_t *p_switch)

Stops an ongoing change of a given multilevel switch.

uint8_t
cc_multilevel_switch_get_current_value(cc_multilevel_switch_t *p_switch)

Returns the current value of a given multilevel switch.

uint8_t
cc_multilevel_switch_get_last_on_value(cc_multilevel_switch_t *p_switch)

Returns the last on-value of a given multilevel switch.

uint8_t

Returns the min value of all multilevel switches.

uint8_t

Returns the max value of all multilevel switches.

void
cc_multilevel_switch_support_cb(struct cc_multilevel_switch_t *p_switch)
bool
cc_multilevel_switch_write(uint8_t multilevel_component_id, cc_multilevel_switch_t *multilevel_switch)
bool
cc_multilevel_switch_read(uint8_t multilevel_component_id, cc_multilevel_switch_t *multilevel_switch)

Enumeration Documentation#

CCMLS_PRIMARY_SWITCH_T#

CCMLS_PRIMARY_SWITCH_T

Enumeration for "Start Level Change" command.

Enumerator
CCMLS_PRIMARY_SWITCH_UP

CCMLS_PRIMARY_SWITCH_UP.

CCMLS_PRIMARY_SWITCH_DOWN

CCMLS_PRIMARY_SWITCH_DOWN.

CCMLS_PRIMARY_SWITCH_RESERVED

CCMLS_PRIMARY_SWITCH_RESERVED.

CCMLS_PRIMARY_SWITCH_NO_UP_DOWN_MOTION

CCMLS_PRIMARY_SWITCH_NO_UP_DOWN_MOTION.


Definition at line 32 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

CCMLS_IGNORE_START_LEVEL_T#

CCMLS_IGNORE_START_LEVEL_T

Enumeration for "Start Level Change" command.

Enumerator
CCMLS_IGNORE_START_LEVEL_FALSE

CCMLS_IGNORE_START_LEVEL_FALSE.

CCMLS_IGNORE_START_LEVEL_TRUE

CCMLS_IGNORE_START_LEVEL_TRUE.


Definition at line 44 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

CCMLS_SECONDARY_SWITCH_T#

CCMLS_SECONDARY_SWITCH_T

Enumeration for "Start Level Change" command.

Enumerator
CCMLS_SECONDARY_SWITCH_INCREMENT

CCMLS_SECONDARY_SWITCH_INCREMENT.

CCMLS_SECONDARY_SWITCH_DECREMENT

CCMLS_SECONDARY_SWITCH_DECREMENT.

CCMLS_SECONDARY_SWITCH_RESERVED

CCMLS_SECONDARY_SWITCH_RESERVED.

CCMLS_SECONDARY_SWITCH_NO_INC_DEC

CCMLS_SECONDARY_SWITCH_NO_INC_DEC.


Definition at line 54 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

Typedef Documentation#

cc_multilevel_switch_t#

typedef struct cc_multilevel_switch_t cc_multilevel_switch_t

Definition at line 38 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_callback_t#

typedef void(* cc_multilevel_switch_callback_t) (struct cc_multilevel_switch_t *p_switch) )(struct cc_multilevel_switch_t *p_switch)

Definition at line 40 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

Function Documentation#

CmdClassMultilevelSwitchStartLevelChange#

JOB_STATUS CmdClassMultilevelSwitchStartLevelChange (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCbFunc, CCMLS_PRIMARY_SWITCH_T primarySwitch, CCMLS_IGNORE_START_LEVEL_T fIgnoreStartLevel, CCMLS_SECONDARY_SWITCH_T secondarySwitch, uint8_t primarySwitchStartLevel, uint8_t duration, uint8_t secondarySwitchStepSize)

Initiates the transmission of a "Multilevel Switch Start Level Change" command.

Parameters
[in]pProfile

pointer to AGI profile or NULL for lifeline

[in]sourceEndpoint

source endpoint

[out]pCbFunc

Callback function to be called when transmission is done/failed.

[in]primarySwitch

Controls the primary device functionality.

[in]fIgnoreStartLevel

Ignore start level.

[in]secondarySwitch

Controls the secondary device functionality.

[in]primarySwitchStartLevel

Start level for the primary device functionality.

[in]duration

The duration from lowest to highest value.

[in]secondarySwitchStepSize

Step size for secondary device functionality.

Returns

  • Status of the job.


Definition at line 82 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

CmdClassMultilevelSwitchStopLevelChange#

JOB_STATUS CmdClassMultilevelSwitchStopLevelChange (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCbFunc)

Initiates the transmission of a "Multilevel Switch Stop Level Change" command.

Parameters
[in]pProfile

pointer to AGI profile

[in]sourceEndpoint

source endpoint

[out]pCbFunc

Callback function to be called when transmission is done/failed.

Returns

  • Status of the job.


Definition at line 102 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

CmdClassMultilevelSwitchSetTransmit#

JOB_STATUS CmdClassMultilevelSwitchSetTransmit (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCbFunc, uint8_t value, uint8_t duration)

Initiates the transmission of a "Multilevel Switch Set" command.

Parameters
[in]pProfile

pointer to AGI profile

[in]sourceEndpoint

source endpoint

[out]pCbFunc

Callback function to be called when transmission is done/failed.

[in]value

Multilevel value.

[in]duration

The duration from current value to the new given value.

Returns

  • Status of the job.


Definition at line 117 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Control.h

cc_multilevel_switch_set#

void cc_multilevel_switch_set (cc_multilevel_switch_t * p_switch, uint8_t value, uint8_t duration)

Sets the value of a given multilevel switch.

Parameters
N/Ap_switch

The switch of which the value is set.

N/Avalue

The value to set.

N/Aduration

The time it takes to reach the value.

This function can be used in an application that might have a button.

Must be used for local actuation only.


Definition at line 53 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_start_level_change#

void cc_multilevel_switch_start_level_change (cc_multilevel_switch_t * p_switch, bool up, bool ignore_start_level, uint8_t start_level, uint8_t duration)

Starts changing the value of a given multilevel switch.

Parameters
N/Ap_switch

The multilevel switch of which the value is changed.

N/Aup

The direction of the change. If true the value will decrease. If false, the value will increase.

N/Aignore_start_level

Decides whether the start level is ignored or not. If set to true, the change will start from the current value. If set to false, the value will start it's change from the given start level.

N/Astart_level

The value to start from if ignore_start_level is set to false.

N/Aduration

The duration of the change.

Must be used for local actuation only.


Definition at line 68 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_stop_level_change#

void cc_multilevel_switch_stop_level_change (cc_multilevel_switch_t * p_switch)

Stops an ongoing change of a given multilevel switch.

Parameters
N/Ap_switch

The multilevel switch of which the change will be stopped.

If no change is ongoing, nothing happens.

Must be used for local actuation only.


Definition at line 82 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_get_current_value#

uint8_t cc_multilevel_switch_get_current_value (cc_multilevel_switch_t * p_switch)

Returns the current value of a given multilevel switch.

Parameters
N/Ap_switch

The multilevel switch of which the value is returned.

Must be used for local actuation only. Returns

  • Current value of the given multilevel switch.


Definition at line 91 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_get_last_on_value#

uint8_t cc_multilevel_switch_get_last_on_value (cc_multilevel_switch_t * p_switch)

Returns the last on-value of a given multilevel switch.

Parameters
N/Ap_switch

The multilevel switch of which the last on-value is returned.

Must be used for local actuation only. Returns

  • Last on value of the given multilevel switch.


Definition at line 100 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_get_min_value#

uint8_t cc_multilevel_switch_get_min_value (void )

Returns the min value of all multilevel switches.

Parameters
N/A

Returns

  • uint8_t Min value of all multilevel switches.


Definition at line 107 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_get_max_value#

uint8_t cc_multilevel_switch_get_max_value (void )

Returns the max value of all multilevel switches.

Parameters
N/A

Returns

  • uint8_t Max value of all multilevel switches.


Definition at line 114 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_support_cb#

void cc_multilevel_switch_support_cb (struct cc_multilevel_switch_t * p_switch)
Parameters
N/Ap_switch

Definition at line 116 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_support_config_get_switches#

cc_multilevel_switch_t * cc_multilevel_switch_support_config_get_switches (void )
Parameters
N/A

Definition at line 118 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_support_config_get_length_switches#

uint8_t cc_multilevel_switch_support_config_get_length_switches (void )
Parameters
N/A

Definition at line 119 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_support_config_get_default_duration#

uint8_t cc_multilevel_switch_support_config_get_default_duration (void )
Parameters
N/A

Definition at line 120 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/inc/CC_MultilevelSwitch_Support.h

cc_multilevel_switch_write#

bool cc_multilevel_switch_write (uint8_t multilevel_component_id, cc_multilevel_switch_t * multilevel_switch)
Parameters
N/Amultilevel_component_id
N/Amultilevel_switch

Definition at line 18 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/src/cc_multilevel_switch_support_io.h

cc_multilevel_switch_read#

bool cc_multilevel_switch_read (uint8_t multilevel_component_id, cc_multilevel_switch_t * multilevel_switch)
Parameters
N/Amultilevel_component_id
N/Amultilevel_switch

Definition at line 19 of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSwitch/src/cc_multilevel_switch_support_io.h