Allocates space for Supervision when used to declare a buffer.

Public Attributes#

ZW_SUPERVISION_GET_FRAME
ZW_APPLICATION_TX_BUFFER

Public Attribute Documentation#

multichanCmdEncap#

uint8_t ZAF_TRANSPORT_TX_BUFFER::multichanCmdEncap[4]

Definition at line 82 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

supervisionGet#

ZW_SUPERVISION_GET_FRAME ZAF_TRANSPORT_TX_BUFFER::supervisionGet

Definition at line 83 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

appTxBuf#

ZW_APPLICATION_TX_BUFFER ZAF_TRANSPORT_TX_BUFFER::appTxBuf

Definition at line 84 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h