Structure with radio parameters for a received frame.

Public Attributes#

Speed for the frame received.

Channel id on which the frame was received.

Z-Wave Header format used in channel frame was received on.

int8_t

Rssi value.

Public Attribute Documentation#

speed#

zpal_radio_speed_t zpal_radio_rx_parameters_t::speed

Speed for the frame received.


Definition at line 410 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

channel_id#

zpal_radio_zwave_channel_t zpal_radio_rx_parameters_t::channel_id

Channel id on which the frame was received.


Definition at line 411 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

channel_header_format#

zpal_radio_header_type_t zpal_radio_rx_parameters_t::channel_header_format

Z-Wave Header format used in channel frame was received on.


Definition at line 412 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rssi#

int8_t zpal_radio_rx_parameters_t::rssi

Rssi value.


Definition at line 413 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h