Z-Wave Serial API#
Modules#
Enumerations#
Firmware update functionality specifics Enum definitions for Firmware Update functionality selector; firmwareUpdateFunction.
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
Macros#
Start Of Frame.
Acknowledge successful frame reception.
Not Acknowledge successful frame reception - please retransmit...
Frame received (from host) was dropped - waiting for ACK.
Enumeration Documentation#
FIRMWARE_UPDATE_NVM_T#
FIRMWARE_UPDATE_NVM_T
Firmware update functionality specifics Enum definitions for Firmware Update functionality selector; firmwareUpdateFunction.
| Enumerator | |
|---|---|
| FIRMWARE_UPDATE_NVM_INIT | |
| FIRMWARE_UPDATE_NVM_SET_NEW_IMAGE | |
| FIRMWARE_UPDATE_NVM_GET_NEW_IMAGE | |
| FIRMWARE_UPDATE_NVM_UPDATE_CRC16 | |
| FIRMWARE_UPDATE_NVM_IS_VALID_CRC16 | |
| FIRMWARE_UPDATE_NVM_WRITE | |
| FIRMWARE_UPDATE_NVM_UNKNOWN | |
nvm_backup_restore_addr_size_t#
nvm_backup_restore_addr_size_t
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
Item value is the size in byte of the address field.
| Enumerator | |
|---|---|
| NVM_BACKUP_RESTORE_ADDR_SIZE | 2 bytes for the legacy NVM backup & restore command |
| NVM_EXT_BACKUP_RESTORE_ADDR_SIZE | 4 bytes for the extended NVM backup & restore command |