UserCode#

Modules#

SUserCode

s_CC_userCode_data_t_

UserCodeEvents

Enumerations#

enum
USER_ID_AVAILABLE = 0x00
USER_ID_OCCUPIED = 0x01
USER_ID_RESERVED = 0x02
USER_ID_NO_STATUS = 0xFE
}

Typedefs#

typedef struct SUserCode
typedef struct s_CC_userCode_data_t_

Struct used to pass operational data to TSE module.

Functions#

bool
CC_UserCode_Write(uint8_t identifier, SUserCode *userCodeData)
bool
CC_UserCode_Read(uint8_t identifier, SUserCode *userCodeData)
CC_UserCode_Set_handler(uint8_t identifier, USER_ID_STATUS id, uint8_t *pUserCode, uint8_t len, uint16_t modifierNodeId)

The User Code Set Command used to set a User Code in the device.

bool
CC_UserCode_getId_handler(uint8_t identifier, USER_ID_STATUS *pId, uint8_t endpoint)

The User Code Get ID.

bool
CC_UserCode_Report_handler(uint8_t identifier, uint8_t *pUserCode, size_t *pLen, uint8_t endpoint)

The User Code Report Command can be used by e.g.

uint8_t

The Users Number Report Command used to report the maximum number of USER CODES the given node supports.

void

Resets the data used by the command class.

void
CC_UserCode_set_usercode(char *new_user_code)

Set the user code to a new value.

CC_UserCode_SupportReport(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, uint8_t userIdentifier, uint8_t userIdStatus, uint8_t *pUserCode, uint8_t userCodeLen, void(*pCallback)(TRANSMISSION_RESULT *pTransmissionResult))

Send a Command Class User code support report.

bool
CC_UserCode_Validate(uint8_t identifier, const uint8_t *pCode, uint8_t len)

Macros#

#define

Minimum length of a user code as defined in SDS12652.

#define

Maximum length of a user code as defined in SDS12652.

Enumeration Documentation#

user_id_status_t#

user_id_status_t

User ID Status.#

The User ID Status field indicates the state of the User Identifier. All other values not mentioned in below list are reserved for future implementation.

Hex

Description

00

Available (not set)

01

Occupied

02

Reserved by administrator

FE

Status not available

Enumerator
USER_ID_AVAILABLE

Available (not set)

USER_ID_OCCUPIED

Occupied.

USER_ID_RESERVED

Reserved by administrator.

USER_ID_NO_STATUS

Status not available.


Typedef Documentation#

USER_ID_STATUS#

typedef user_id_status_t USER_ID_STATUS

SUserCode#

typedef struct SUserCode SUserCode

s_CC_userCode_data_t#

typedef struct s_CC_userCode_data_t_ s_CC_userCode_data_t

Struct used to pass operational data to TSE module.


Function Documentation#

CC_UserCode_Migrate#

void CC_UserCode_Migrate ()

CC_UserCode_Write#

bool CC_UserCode_Write (uint8_t identifier, SUserCode * userCodeData)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aidentifier
SUserCode *N/AuserCodeData

CC_UserCode_Read#

bool CC_UserCode_Read (uint8_t identifier, SUserCode * userCodeData)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aidentifier
SUserCode *N/AuserCodeData

CC_UserCode_Set_handler#

e_cmd_handler_return_code_t CC_UserCode_Set_handler (uint8_t identifier, USER_ID_STATUS id, uint8_t * pUserCode, uint8_t len, uint16_t modifierNodeId)

The User Code Set Command used to set a User Code in the device.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]identifier

User Identifier.

USER_ID_STATUS[in]id

user Id status.

uint8_t *[in]pUserCode

pointer to UserCode data.

uint8_t[in]len

UserCode data.

uint16_t[in]modifierNodeId

Node ID of the requesting node.

Returns

  • command handler return code


CC_UserCode_getId_handler#

bool CC_UserCode_getId_handler (uint8_t identifier, USER_ID_STATUS * pId, uint8_t endpoint)

The User Code Get ID.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]identifier

User Identifier.

USER_ID_STATUS *[out]pId

pointer to return Id.

uint8_t[in]endpoint

is the destination endpoint

Returns

  • status valid boolean.


CC_UserCode_Report_handler#

bool CC_UserCode_Report_handler (uint8_t identifier, uint8_t * pUserCode, size_t * pLen, uint8_t endpoint)

The User Code Report Command can be used by e.g.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]identifier

User Identifier.

uint8_t *[out]pUserCode

pointer to UserCode data.

size_t *[out]pLen

length UserCode data.

uint8_t[in]endpoint

is the destination endpoint

a door lock device to send a report either unsolicited or requested by the User Code Get Command. Returns

  • status valid boolean.


CC_UserCode_UsersNumberReport_handler#

uint8_t CC_UserCode_UsersNumberReport_handler (uint8_t endpoint)

The Users Number Report Command used to report the maximum number of USER CODES the given node supports.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]endpoint

is the destination endpoint

The Users Number Report Command can be send requested by the Users Number Get Command. Returns

  • maximum number of USER CODES.


CC_UserCode_reset_data#

void CC_UserCode_reset_data (void )

Resets the data used by the command class.

Parameters
TypeDirectionArgument NameDescription
voidN/A

CC_UserCode_set_usercode#

void CC_UserCode_set_usercode (char * new_user_code)

Set the user code to a new value.

Parameters
TypeDirectionArgument NameDescription
char *[in]new_user_code

The new user code, must be under the length of USERCODE_MAX_LEN


CC_UserCode_SupportReport#

JOB_STATUS CC_UserCode_SupportReport (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, uint8_t userIdentifier, uint8_t userIdStatus, uint8_t * pUserCode, uint8_t userCodeLen, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCallback)

Send a Command Class User code support report.

Parameters
TypeDirectionArgument NameDescription
AGI_PROFILE *[in]pProfile

pointer to AGI profile

uint8_t[in]sourceEndpoint

source endpoint

uint8_t[in]userIdentifier

user identifier

uint8_t[in]userIdStatus

user Id status

uint8_t *[in]pUserCode

user code

uint8_t[in]userCodeLen

length of user code

void(*)(TRANSMISSION_RESULT *pTransmissionResult)[out]pCallback

callback function returning status destination node receive job.

Returns

  • status on the job.


CC_UserCode_Validate#

bool CC_UserCode_Validate (uint8_t identifier, const uint8_t * pCode, uint8_t len)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aidentifier
const uint8_t *N/ApCode
uint8_tN/Alen

Macro Definition Documentation#

USERCODE_MIN_LEN#

#define USERCODE_MIN_LEN
Value:
4

Minimum length of a user code as defined in SDS12652.


USERCODE_MAX_LEN#

#define USERCODE_MAX_LEN
Value:
10

Maximum length of a user code as defined in SDS12652.