ZWavePlusInfo#
Modules#
Functions#
Returns the Installer and User Icon Type configuration of the root device.
Returns the number of endpoints defined in the application command class configuration.
Returns the Installer and User Icon Type configuration of the given 'endpoint'.
Function Documentation#
cc_zwave_plus_info_config_get_root_icons#
zw_plus_info_config_icons_t * cc_zwave_plus_info_config_get_root_icons (void )
Returns the Installer and User Icon Type configuration of the root device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
- Pointer to struct contains the icon types. 
cc_zwave_plus_info_config_get_endpoint_count#
uint8_t cc_zwave_plus_info_config_get_endpoint_count (void )
Returns the number of endpoints defined in the application command class configuration.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
In case of no zw_cc_zwaveplusinfo is given in the config, returns with 0.
Returns
- the number of endpoints. 
cc_zwave_plus_info_config_get_endpoint_entry#
zw_plus_info_config_icons_t * cc_zwave_plus_info_config_get_endpoint_entry (uint8_t endpoint)
Returns the Installer and User Icon Type configuration of the given 'endpoint'.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | the index of the requested endpoint. First endpoint index starting by 1. | 
Returns
- Pointer to struct contains the icon types for the given endpoint.