Radio Profile containing region, baud rate, and wakeup interval for this device.
Public Attributes#
Region in which this system operates.
Wakeup interval for the radio.
Primary Long Range Channel.
Longe Range channel selection mode.
Long Range channel configuration.
LBT Threshold for Transmit backoff in dBm.
Z-Wave Transmit Power in deci dBm.
Adjustment for antenna gain in deci dBm.
Max transmit power for Z-Wave LR in deci dBm.
Pointer to function called by RF on Rx Completion.
Pointer to function called by RF on Tx Completion.
Pointer to function called by RF on Region change.
Pointer to function called by RF on fatal Assert.
Pointer to structure where to RF Statistics are placed.
Enable radio debugging which is vendor specific.
Pointer to receive handler.
Application type.
Public Attribute Documentation#
primary_lr_channel#
zpal_radio_lr_channel_t zpal_radio_profile_t::primary_lr_channel
Primary Long Range Channel.
lr_channel_auto_mode#
bool zpal_radio_profile_t::lr_channel_auto_mode
Longe Range channel selection mode.
active_lr_channel_config#
zpal_radio_lr_channel_config_t zpal_radio_profile_t::active_lr_channel_config
Long Range channel configuration.
Set only when radio chip configuration is updated. Used to check that requested channel configuration is different than the active one.
listen_before_talk_threshold#
int8_t zpal_radio_profile_t::listen_before_talk_threshold
LBT Threshold for Transmit backoff in dBm.
tx_power_adjust#
zpal_tx_power_t zpal_radio_profile_t::tx_power_adjust
Adjustment for antenna gain in deci dBm.
tx_power_max_lr#
zpal_tx_power_t zpal_radio_profile_t::tx_power_max_lr
Max transmit power for Z-Wave LR in deci dBm.
rx_cb#
zpal_radio_callback_t zpal_radio_profile_t::rx_cb
Pointer to function called by RF on Rx Completion.
tx_cb#
zpal_radio_callback_t zpal_radio_profile_t::tx_cb
Pointer to function called by RF on Tx Completion.
region_change_cb#
zpal_radio_callback_t zpal_radio_profile_t::region_change_cb
Pointer to function called by RF on Region change.
assert_cb#
zpal_radio_callback_t zpal_radio_profile_t::assert_cb
Pointer to function called by RF on fatal Assert.
network_stats#
zpal_radio_network_stats_t* zpal_radio_profile_t::network_stats
Pointer to structure where to RF Statistics are placed.
radio_debug_enable#
uint8_t zpal_radio_profile_t::radio_debug_enable
Enable radio debugging which is vendor specific.
receive_handler_cb#
zpal_radio_receive_handler_t zpal_radio_profile_t::receive_handler_cb
Pointer to receive handler.