Z-Wave SDK Version 8.0.2 - Release Notes#
Simplicity SDK Version 2025.12.0
Z-Wave and Z-Wave Long Range SDK are designed to meet the demands of the future smart home and beyond, where increasing needs for more sensors and battery-operated devices require both long range and low power. Context-aware environments are the next evolution in the smart home market, and they require technologies that have been optimized specifically for these applications.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Addressing the increasing demands for low power in battery-operated devices, the Z-Wave stack is now implemented independently from the platform power state (e.g., energy modes: EM0, EM1, EM1P, EM2, EM3/EM4). This architectural improvement reduces overall stack power consumption during radio events by leveraging the EM1P power state during radio operations instead of EM1. Additionally, using
sl_power_managerAPIs from application code will no longer interfere with Z-Wave stack radio logic. For more details, refer to the Important Changes section.The Z-Wave Long Range TX output power algorithm is refactored. It now tracks independently all the Z-Wave Long Range end devices. It is backward-compatible with the previous algorithm.
The 9.6 kbps PHY is used only if an end device in the network is not able to operate at a higher modulation rate (40 kbps or 100 kbps).
API Changes#
The
zpal_power_managermodule is removed from the Z-Wave Silicon Labs PAL. It is replaced by two entities:A new
zw_shutdown_managercomponent. This module is responsible for sending a never listening end device to the EM4 power state. Requirements can be added by the application to prevent that transition, similarly to thesl_power_managercomponent.In the
zpal_radioPAL layer, new APIszpal_radio_request_stay_awakeandzpal_radio_revoke_stay_awakehandle requests to maintain an RX radio state in the stack.
The Packet Trace Interface (PTI) enablement relies on the standard
sl_rail_util_pticomponent instead of specific Z-Wave stack APIs.
Bug Fixes#
Below are important bugs fixed in this release. For a complete list, refer to this section.
The previous Z-Wave Long Range TX output power algorithm had an issue in the low output power range. It would revert to transmitting at the maximum output power. The issue is addressed in the newer implementation.
The FLiRS end device radio behavior was impacted negatively by the use of the
zpal_pm_stay_awake()API. It would prevent the Z-Wave stack from properly behaving and acknowledging beam events. With the power management refactoring, this is no longer a concern. The Z-Wave stack behaves independently from application power management decisions.NLS Support won't be enabled by default anymore. Added optional component (zw_s2_nls_support) to enable Network Level Security (NLS) support advertisement in the KEX Report during S2 inclusion. This allows alpha testing of NLS while avoiding certification issues when the feature is not certified.
Margin of the dynamic Tx power algorithm was too aggressive. Set a new margin to 6dBm to reduce the probability of failure on first attempt.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
The Z-Wave stack is now independent from the power state of the platform, meaning that using sl_power_manager APIs will not interfere with Z-Wave stack logic. It improves the stack power consumption during radio events, leveraging the EM1P power state. Refer to Important Changes for additional information.
Note: This improvement has implications on the application. It is now responsible to keep the EFR32 host awake if required. The Z-Wave stack only handles the radio state.
Create an API to customize the DTPA noise margin from the application. Note that the noise margin is not stored in NVM. So the application should set the customized value after each init phase.
Enhancements#
The Z-Wave Long Range TX output power algorithm is refactored. It now tracks independently of all Z-Wave Long Range end devices. It is backward-compatible with the previous algorithm.
The 9.6 kbps PHY is used only if an end device in the network is not able to operate at a higher modulation rate (40 kbps or 100 kbps).
The function CC_Configuration_SetValue(), previously only declared without an implementation, has been implemented.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
New API Signature
Deprecated API replaced by this (if any) </thead> <tbody>
CC_UserCredential_send_association_report
CC_UserCredential_AssociationReport_tx
ZW_DCDC_CONFIG1
ZW_EM4_PIN_RETENTION_MODE
SL_DEVICE_INIT_EMU_EM4_PIN_RETENTION_MODE
ZW_EM4_INITIAL_STATE
SL_DEVICE_INIT_EMU_EM4_STATE
ZW_EM23_VOLTAGE_SCALE
ZW_EM4_RETAIN_LFXO
SL_DEVICE_INIT_EMU_EM4_RETAIN_LFXO
ZW_EM4_RETAIN_LFRCO
SL_DEVICE_INIT_EMU_EM4_RETAIN_LFRCO
ZW_EM4_RETAIN_ULFRCO
SL_DEVICE_INIT_EMU_EM4_RETAIN_ULFRCO
zw_shutdown_manager_add_lock
zw_power_manager_lock2
zpal_pm_lock2
zw_shutdown_manager_take_temporary_lock
zw_power_manager_relock2
zpal_pm_relock2
zw_shutdown_manager_release_lock
zw_power_manager_lock_cancel2
zpal_pm_lock_cancel2
zw_shutdown_manager_init
zw_power_manager_init2
zpal_pm_init2
ZW_dtpa_set_noise_margin
None
ZW_dtpa_get_noise_margin
None </tbody>
¹ The value of ZW_DCDC_CONFIG is currently not applied by the Z-Wave stack.
² The exact replacements for these Power Manager APIs depend on your use case:
For controlling the power state (i.e. EM state) of the ARM core, use the
sl_power_managerAPI.To maintain the Z-Wave radio in an active listening state during periods when the application itself is not transmitting, use the
zpal_radioAPI.To prevent the device from entering deep sleep mode, use the
zw_shutdown_managerAPI.
Note that the new lock behavior is significantly different from the previous Power Manager APIs.
For more details, refer to Important Changes and Migration Guide.
Modified APIs#
Old API
Modified API </thead> <tbody>
zpal_tx_power_t
zpal_tx_power_decidbm_t
ZW_TX_POWER_10DBM
ZW_TX_POWER_100_DDBM
ZW_TX_POWER_14DBM
ZW_TX_POWER_140_DDBM
ZW_TX_POWER_20DBM
ZW_TX_POWER_200_DDBM
EZWAVECOMMANDSTATUS_GET_ROUTING_TABLE_LINE
EZWAVECOMMANDSTATUS_GET_NEIGHBOR_TABLE_LINE
EZWAVECOMMANDTYPE_GET_ROUTING_TABLE_LINE
EZWAVECOMMANDTYPE_GET_NEIGHBOR_TABLE_LINE
SUPPORT_GET_ROUTING_TABLE_LINE
SUPPORT_GET_NEIGHBOR_TABLE_LINE </tbody>
Removed APIs#
Removed API | Was Deprecated? |
|---|---|
zw_power_manager_is_active | No |
zw_power_manager_init | No |
zw_power_manager_lock | No |
zw_power_manager_relock | No |
zw_power_manager_lock_cancel | No |
zpal_get_max_timeout | No |
zpal_pm_lock_is_active | No |
zpal_pm_init | No |
zpal_pm_lock | No |
zpal_pm_relock | No |
zpal_pm_lock_cancel | No |
zpal_pm_halt | No |
zpal_pm_register_domain | No |
zpal_zw_pm_event_handler | No |
zpal_radio_debug_configure | No |
zpal_radio_is_debug_enabled | No |
EZWAVECOMMANDTYPE_ZW_GET_PTI_CONFIG | No |
EZWAVECOMMANDSTATUS_ZW_GET_PTI_CONFIG | No |
Deprecated APIs#
Deprecated API | Planned Removal Date (if any) | Replacement API Name (if any) |
|---|---|---|
CC_UserCredential_send_association_report | TBD | CC_UserCredential_AssociationReport_tx |
Bug Fixes#
<col width="10%"> <col width="45%"> <col width="20%"> <col width="25%"> </colgroup> <thead>
ID
Issue Description
GitHub / Salesforce Reference (if any)
Affected Software Variants, Hardware, Modes, Host Interfaces </thead> <tbody>
1542556
Fixed an issue that prevented the modification of credential data via the CLI. All-zero PIN Code credentials (e.g. 0000) are now rejected by default.
None
ZAF / User Credential Command Class
1525543
Fixed lower limit of configuration ranges in CC Binary Switch duration, User Credential CC max credential slots, and minimum and maximum credential data length to allow values of 0.
None
ZAF / User Credential Command Class, Binary Switch Command Class
1516742
Fixed User Credential Association Reports not being advertised in the list of Lifeline notifications and not being sent to the required Lifeline destinations.
None
ZAF / User Credential Command Class
1489288
Fixed applications supporting the User Credential Command Class not reporting support for name encodings ASCII, Extended ASCII, and UTF-16. This applies changes from the 2025A specification.
None
ZAF / User Credential Command Class
1488041
A Credential Report with the status "Credential Unchanged" is now returned if no credentials are deleted after a bulk credential deletion request is received over the air. This applies changes from the 2025A specification.
None
ZAF / User Credential Command Class
1480294
Fixed the s_colorComponent structure to be compatible with the zaf_config_t.
None
ZAF / Color Switch Command Class
1473325
Slow refresh has been enabled by default in Central Scene V3 according to the specification.
None
Central Scene Command Class
zwave_soc_wall_controller
1432659
Fixed an issue when too many reports are sent when multiple buttons are pressed at once.
None
All examples
1556171
Multilevel Sensor Command Class support has been extended to include all sensor types and scales defined by the specification. If auto-generating sources from .cc_config files fails, no error message is displayed. It is recommended to run the CC Configurator manually (see DevTools/cc_configurator/README).
None
Multilevel Sensor Command Class
1490329
User-defined configurations in SLC project files related to the Energy Management Unit had not been applied due to the Z-Wave stack initialization process overriding them with hard-coded values. These configurations are now configurable via the Z-Wave Core Component and applied correctly except for the DC/DC Converter Mode (ZW_DCDC_CONFIG), which is still hard-coded.
None
All examples
1356409
Fixed an issue where the Serial API controller would not acknowledge the "Initiate Shutdown" command.
SF case 00320844
Serial API controller
1298116
The Serial API controller could mistake an Explorer Autoinclusion frame as an Application Frame, notifying the host with "junk" data. The packet is now properly handled.
SF case 00315326
Serial API controller
1390101
Fixed an issue preventing the configuration of a TX output power above +14 dBm in the Serial API controller application.
None
ZPAL
1516616
Fixed an issue where the Z-Wave Long Range TX output power algorithm would transmit at maximum power while it was supposed to transmit at a negative TX power.
None
ZPAL radio
1358615
Addressed a behavior where a FLiRS device would not be able to acknowledge a beam when the zpal_pm_stay_awake() API was used.
SF case 00320854
ZPAL
378359
Previously, KEX Fail messages were sent without being secure. They are now sent encrypted with the same level of encryption as the frame at that point of inclusion. The fix aligns with the behavior to the Z-Wave specification.
None
Z-Wave stack
1325755
Removed an unnecessary duplicate message during the S2 bootstrapping process when S2 Authenticated mode is used.
None
Z-Wave stack
1600768
NLS Support was advertised in KEX Report for all end node firmwares since version 7.23.0 even when the feature was not certified, which could cause certification issues. Added optional component (zw_s2_nls_support) to allow users to choose whether to enable NLS support for alpha testing.
S2V2, end nodes
1603657
Restore the fragmented LR beam length to 3s (it was set to 2s from SDK version 7.20 onwards). The change had introduced a regression where FLiRS devices (configured for 900ms wakeup period) would miss about 10% of the beams.
None
Z-Wave stack
1605311
Fixed an issue that prevented controllers from handling beam ACK when only 1 fragment was remaining.
None
Z-Wave stack
1604659
Fixed an issue where the FLiRS device did not wait for the end of the fragment to send the beam ACK.
None
ZPAL radio </tbody>
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
<col width="10%"> <col width="40%"> <col width="10%"> <col width="10%"> <col width="20%"> <col width="10%"> </colgroup> <thead>
Example Name
Changes
Supported Software Variants if applicable
Supported Modes
Supported OPNs / Boards / OPN Combinations
Supported Host Interfaces </thead> <tbody>
zwave_soc_sensor_pir
Removed unused device init config: SL_DEVICE_INIT_LFXO_TIMEOUT
N/A
OPN: All Z-Wave supported 800 series OPNs
All Z-Wave supported 800 series boards
N/A
All examples
The Energy Management Unit related configurations, previously set in the SLC project files, had been overridden by system_startup_core during the stack init phase. To maintain their visibility, they were moved to the configuration of the zw_core component in a new, hardware-specific header file.
N/A
OPN: All Z-Wave supported 800 series OPNs
All Z-Wave supported 800 series boards
N/A
zwave_soc_sensor_pir, zwave_soc_multilevel_sensor
The Sensor PIR and Multilevel Sensor applications now support the S0 security scheme (Security Command Class V1). See Note below this table.
N/A
OPN: All Z-Wave supported 800 series OPNs
All Z-Wave supported 800 series boards
N/A </tbody>
Note: The S0 security scheme enablement is introduced regressions on the S0_InvalidNetworkKeySet_Rev01 and S0_SettingNewNetworkKey_Rev01 CTT tests. Currently, these are identified as test-related errors. Clarification is in progress with the Z-Wave Alliance and test house.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
<col width="10%"> <col width="40%"> <col width="15%"> <col width="20%"> <col width="15%"> </colgroup> <thead>
ID
Issue or Limitation Description
GitHub / Salesforce Reference (if any)
Workaround (if any)
Affected Software Variants, Hardware, Modes, Host Interfaces </thead> <tbody>
1556587
Endpoints are handled incorrectly in the Multilevel Sensor Command Class implementations: the sensor types and scales configured for the first endpoint are mirrored to subsequent endpoints, overriding their configuration.
Currently not available.
ZAF / Multilevel Sensor Command Class
1568087
The configuration value for DC/DC Converter Mode (ZW_DCDC_CONFIG) is not applied.
Currently not available.
All Z-Wave applications
1399709
Reported S2 command class version remains 1 until certification covers S2v2.
Currently not available.
All Z-Wave applications
369430
All S2 multicast frames are sent using verified delivery S2_TXOPTION_VERIFY_DELIVERY whether or not a response is expected.
Change source code depending on the frame sent.
ZAF
1067228
Zniffer on BRD4204D does not detect LR wakeup beams.
Use different board for sniffing LR wakeup beams.
zwave_ncp_zniffer
1556296
The never listening device type activity profile is modified during SmartStart inclusion. It results in improved power consumption when the device is not transmitting smart start frames but additional power consumption during the SmartStart communications (typically from 1.22 µA to 1.89 µA).
Never listening device type.
1568316
In regions that leverage fragmented beams (Japan, Korea, and Long Range), the acknowledgement from the Frequently Listening device can be sent at the end of the fragmented beam instead of when the first fragment is received. This results in an added delay for the end device to notify the beaming device.
Frequently Listening device type. </tbody>
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
Click here for the migration guide for deprecated, removed, and modified items.
Using This Release#
Installation and Use | Help and Feedback
Installation and Use#
To upgrade your existing software with this release, see instructions in the Migration Guide.
To run your first demo, see our Z-Wave Getting Started for End Devices.
To learn more about the software in this release, dive into our Z-Wave online documentation.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note:Ask AI is experimental.
- Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.