Migration Guide#

  This guide shows how to migrate projects from previous SDKs to a newer one.

8.1.0#

Sleeptimer peripheral configuration#

In 8.1.0, Z-Wave applications on Series 2 must use SL_SLEEPTIMER_PERIPHERAL_DEFAULT (SYSRTC) for the platform sleeptimer. BURTC is reserved for Z-Wave power management (zw_shutdown_manager).

When upgrading from an older SDK, the automated upgrade (upgrade.slcu) sets:

  • SL_SLEEPTIMER_PERIPHERAL to SL_SLEEPTIMER_PERIPHERAL_DEFAULT

CLI no longer uses app_log#

CLI components are now designed to use sl_iostream for both input and output. For old projects that are using CLI components with app_log API, the automated upgrade (slcu) will add a dependency on app_log. If you don't want to use app_log in your CLI files, you should:

  • Include sl_iostream.h and sl_iostream_handles.h instead of app_log.h

  • Load the correct iostream (e.g. sl_iostream_t *stream = sl_iostream_get_handle("vcom");)

  • Replace calls to app_log_info(...) with sl_iostream_vprintf(stream, ...) Note that if you get the error "app_log.h: No such file or directory" after the migration, that means your are missing the app_log component in your projet. It can be easly fixed by installing the app_log component in your project.

DC/DC configuration (<tt>ZW_DCDC_CONFIG</tt>)#

In 8.1.0, ZW_DCDC_CONFIG in zw_hardware_config.h (or Project Configurator) is applied when the radio platform initializes the DC/DC at startup. In 8.0.0 that setting was ignored and the firmware always used EDCDCMODE_AUTO.

The setting chooses how the on-chip DC/DC runs at startup:

  • EDCDCMODE_AUTO (default): the chip picks bypass vs regulation from the supply level. Fine for most boards.

  • EDCDCMODE_BYPASS: always bypass. Try this if sleep current stays high after transmit on a very low battery (roughly 2.1–2.5 V).

  • EDCDCMODE_DCDC_LOW_NOISE: always regulate for lower noise. Use when the battery or regulator always stays above the minimum the DC/DC needs.

8.0.0#

zpal_power_manager APIs migration#

Following the removal of zpal_power_manager, here are the APIs you need to remove from your code:

  • zpal_pm_lock, zpal_pm_relock, zpal_get_max_timeout, zpal_pm_lock_is_active, zpal_pm_register_domain, zpal_pm_lock_cancel, zpal_zw_pm_event_handler, zpal_pm_halt

  • zw_power_manager_lock, zw_power_manager_relock, zw_power_manager_is_active, zw_power_manager_lock_cancel, zw_power_manager_init

These APIs can be replaced with three different modules depending on your usage:

  • If you want to handle the power manager "state" (e.g., EM state) of the ARM core, you can now use the dedicated platform APIs of sl_power_manager.

  • If you want to maintain the Z-Wave radio in an active state (RX active when no TX is in progress), you should use the new dedicated APIs zpal_radio_request_stay_awake or zpal_radio_update_stay_awake instead of the previous API: zpal_pm_lock(ZPAL_PM_TYPE_USE_RADIO).

    • To revoke a previous request, use zpal_radio_revoke_stay_awake.

  • If you want to maintain deep sleep mode, equivalent to the previous zpal_pm_lock(ZPAL_PM_TYPE_DEEP_SLEEP), you can now use the new component module called zw_shutdown_manager. The logic of this module works the same way as sl_power_manager: adding or subtracting 1 to a global counter based on lock requests. When count == 0, the module considers the device ready to enter shutdown mode (EM4).

APIs of this new module are:

  • zw_shutdown_manager_add_lock to request a lock

  • zw_shutdown_manager_release_lock to release a lock

  • zw_shutdown_manager_take_temporary_lock to take a temporary lock for a given duration

TxPower type and definitions clarification#

Some type and definitions have been renamed to avoid confusion:

Old name

New name

zpal_tx_power_t

zpal_tx_power_decidbm_t

ZW_TX_POWER_10DBM

ZW_TX_POWER_100_DDBM

ZW_TX_POWER_14DBM

ZW_TX_POWER_140_DDBM

ZW_TX_POWER_20DBM

ZW_TX_POWER_200_DDBM

If your application uses these definitions, you need to replace them with the new names.

Energy modes#

Some peripherals may not work in the newly introduced EM1P energy mode (for example, TIMER0). To address this, an EM1 requirement may be added to the power manager module by the application.

To add an EM1 lock to the application, include the power manager header, and call the following function during initialization.

#include "sl_power_manager.h"

sl_power_manager_add_em_requirement(SL_POWER_MANAGER_EM1);

Timers used by the PWM component in Led Bulb and Power Strip applications only work in EM1 mode, therefore, updating these applications require the above manual changes to be made.

Hardware Configuration#

A new hardware configuration API has been introduced, allowing to control the Energy Management Unit (EMU).
The following configuration values, previously defined in the SLC project files (.slcp) had been hard-coded to specific values in prior releases, regardless of the user-configured values.
These values can now be set via the Z-Wave Core Component (if using the GUI) or via the configuration header zw_hardware_config.h:

Old configuration name

New configuration name

-

ZW_DCDC_CONFIG*

SL_DEVICE_INIT_EMU_EM4_PIN_RETENTION_MODE

ZW_EM4_PIN_RETENTION_MODE

SL_DEVICE_INIT_EMU_EM4_STATE

ZW_EM4_INITIAL_STATE

-

ZW_EM23_VOLTAGE_SCALE

SL_DEVICE_INIT_EMU_EM4_RETAIN_LFXO

ZW_EM4_RETAIN_LFXO

SL_DEVICE_INIT_EMU_EM4_RETAIN_LFRCO

ZW_EM4_RETAIN_LFRCO

SL_DEVICE_INIT_EMU_EM4_RETAIN_ULFRCO

ZW_EM4_RETAIN_ULFRCO

  • The ZW_DCDC_CONFIG configuration value is still hard-coded to EDCDCMODE_AUTO, regardless of the value of this setting. A workaround is currently not available. SDK 8.1.0 applies this setting; see DC/DC configuration (`ZW_DCDC_CONFIG`).

RAIL Power Manager Initialization#

FLiRS applications (e.g. the Door Lock Keypad application) require the RAIL Power Manager Initialization configuration to be enabled. To do this on an upgraded project, set the value to 1 in the config/sl_rail_util_power_manager_init_config.h file:

#define SL_RAIL_UTIL_RAIL_POWER_MANAGER_INIT 1

7.24.1#

How to migrate the Wall Controller sample application#

The configuration macro SHORT_BUTTON_PRESS_DURATION was renamed to SHORT_BUTTON_PRESS_DURATION_MS.

Modify the app_button_press_btn_0_handler function to use the new macro:

- sl_sleeptimer_start_timer_ms(&my_sleeptimer_handle, SHORT_BUTTON_PRESS_DURATION, sleeptimer_cb, NULL, 0, 0);
+ sl_sleeptimer_start_timer_ms(&my_sleeptimer_handle, SHORT_BUTTON_PRESS_DURATION_MS, sleeptimer_cb, NULL, 0, 0);

7.24.0#

Power Manager#

It is strongly recommended that applications rely on the zw_power_manager abstraction and do not use the zpal_pm APIs, see zw_power_manager_ids.h for available wrapper.

  • Note

    • : an application must call zw_power_manager_init prior to using zw_power_manager APIs. If not, the lock operation will be ignored. This call is introduced in ZAF_Init(). For NCP Serial API (End Device/Controller) applications, it is done in ApplicationInit() as these apps do not depend on ZAF layer. If your application does not depend on ZAF, please add this function call prior to using zw_power_manager APIs.

    If the application still needs to use zpal_pm API, then: Any application code previously using zpal_pm_register, zpal_pm_stay_awake, zpal_pm_cancel are expected to align with the following rules:

  • zpal_pm_register is deprecated. Instead, a power lock ID must be defined in either ZPAL_PM_AppRadioID or ZPAL_PM_AppDeepSleepID. This ID must be used in all operations of this power lock.

  • Any call to zpal_pm_stay_awake, zpal_pm_cancel should now be aligned with zw_power_manager_(lock/relock/lock_cancel)

Watchdog#

Apps are now responsible for the watchdog activation by calling "zpal_watchdog_init" and "zpal_enable_watchdog" functions consecutively. (see sample applications for reference).

Logging System#

The Debug Print component was replaced by the ZPAL Log API, which allows filtering log messages by source component and log level.

To ensure compatibility with the new logging system, some files relying on Debug Print may have to be modified by including the header zpal_log.h, replacing DPRINT and DPRINTF with ZPAL_LOG and removing any references to the old component.

To enable debug output, either use the Configure button of the Z-Wave Log component in Simplicity Studio or edit zw_log_config.h directly in the project's config directory:

  • configure the output channels for the 4 log levels (debug, info, warning, error) by setting ZW_LOG_CHANNEL_<log level> to an existing IO Stream instance (vcom, rtt, etc.)

  • set the relevant defines ZPAL_LOG_ENABLE_<component name> to 1.

To extend the ZPAL Log API with a new component, add a new entry to the enum zpal_log_component_t and update the helper macros in zpal_log_internal.h.

main.c#

The file main.c is now generated by the System Setup (sl_main) component. If you previously extended this file with your own initialization functions, these should be relocated and registered using the Event Handler API. The main.c file should then be removed.

For more information, refer to the documentation for System Initialization and Action Processing.

User Credential Command Class#

If your project uses or redefines the CC_UserCredential_move_credential_and_report function: remove the destination_credential_slot parameter and rename the source_credential_slot parameter to credential_slot.

The following structs were renamed:

Old name

New name

u3c_user

u3c_user_t

u3c_credential

u3c_credential_t

u3c_event_data_validate

u3c_event_data_validate_t

u3c_event_data_learn_read_done

u3c_event_data_learn_read_done_t

u3c_credential_metadata

u3c_credential_metadata_t

u3c_credential_learn_event_data

u3c_event_data_learn_start_t

Application Specific Hardware Initialization#

In app.c, ensure that the function app_hw_init() is invoked by the ApplicationInit function (after ZAF_Init, if present). In an unmodified project, this can be done by removing the #if preprocessor directives:

- #if (!defined(SL_CATALOG_SILICON_LABS_ZWAVE_APPLICATION_PRESENT) && !defined(UNIT_TEST))
    #include "app_hw.h"
- #endif
- #if (!defined(SL_CATALOG_SILICON_LABS_ZWAVE_APPLICATION_PRESENT) && !defined(UNIT_TEST))
    app_hw_init();
- #endif

Waking Button Press Detection for Sleeping Applications#

If your application has the Sleeping Reporting role type, extend the project's .slcp file with the following configuration and regenerate the project:

configuration:
  (...)
  - name: APP_BUTTON_PRESS_WAKEUP_DELAY
    value: 46 # Average time for Sleep Timer to start after a reset when built in ocelot
    condition: [device_sdid_210]
  - name: APP_BUTTON_PRESS_WAKEUP_DELAY
    value: 285 # Average time for Sleep Timer to start after a reset when built in margay
    condition: [device_sdid_235]

This will ensure that the application detects the correct button press duration when waking up from a sleeping state via a button press.

RAIL Power Manager Initialization#

The SL_RAIL_UTIL_RAIL_POWER_MANAGER_INIT configuration value should be set to 0 for the Door Lock Keypad application and to 1 for all other applications. During the SDK update, this configuration value is automatically set to 1 for all applications, including Door Lock Keypad. Therefore, for the Door Lock Keypad application, it must be set manually to 0; other applications are handled automatically.

This is necessary for a proper initialization sequence of the power manager component for all applications.

How to upgrade sample applications#

In the following sections, an example is shown about the upgrade steps of each sample application.

Steps for an SDK upgrade:#

  1. Upgrade SDK for the selected application.

  2. Make changes according to the steps described in the current document.

  3. Regenerate the application (force regeneration).

  4. Build the application

Note: This guide is not exhaustive. Please ensure that any changes you make follow the steps outlined above.

General steps for all applications#

All .c files#
  • Remove #include "DebugPrint.h" and #include "DebugPrintConfig.h"

  • Remove any references to DEBUGPRINT because it is deprecated.

  • Replace all DPRINT(...) and DPRINTF(...) API calls to ZPAL_LOG_DEBUG(ZPAL_LOG_APP, ...).

  • Replace DebugPrintf with ZPAL_LOG_INFO(ZPAL_LOG_APP, ...).

  • Remove DebugPrintConfig(...) calls.

  • Add #include "zpal_log.h" if ZPAL_LOG_... calls are used.

app.c of all applications#
  • Remove m_aDebugPrintBuffer variable and its references.

  • Add zpal_watchdog_init() before zpal_enable_watchdog(true) in ApplicationInit.

<project_name>.slcp#
  • Remove sl_system and sl_system_kernel components if present.

  • Add sl_main component.

  • Remove main.c from source files.

    • This will be generated by the sl_main component after project regeneration.

    • If main.c was modified, it is advised to move custom code to a different file, e.g. app.c.

  • Set the configuration value SL_RAIL_UTIL_RAIL_POWER_MANAGER_INIT to 0 for Door Lock Keypad, and to 1 for all the other applications.

  • Add clock_manager component.

  • Add the following configuration values:

    • name: SL_CLOCK_MANAGER_WDOG0CLK_SOURCE, value: CMU_WDOG0CLKCTRL_CLKSEL_LFRCO

  • Add the following provides:

    provides:
      - name: zwave_sample_application
      - name: <project_name> # e.g. zwave_soc_power_strip
    

NCP Zniffer and Zniffer PTI#

NCP Zniffer and Zniffer PTI applications were merged into one application. Now, NCP Zniffer contains both applications' functionalities. It is not possible to upgrade these applications directly. Instead, please create a new project using the latest SDK and manually transfer any changes made in the previous project to the new one.

NCP Serial API Controller#

SDK upgrades are not supported for this application. To migrate, please create a new project using the latest SDK and manually transfer any changes from the previous project to the new one.

Door Lock Keypad#

app.c#
  • Add #include "app_pm_transition_event.h"

  • Add these lines after RadioConfig = zaf_get_radio_config();

    #ifdef SL_CATALOG_ZW_PM_TRANSITION_EVENT_PRESENT
      // register callback from power manager transitions
      ZW_PmTransitionEventInit();
    #endif
    
  • Remove zw_cli_sleeping_util_prevent_sleeping_timeout(ZW_CLI_SLEEPING_WAKEUP_TIME_AFTER_RESET);

  • CLI baud rate was changed to 9600, which enables the device to receive CLI commands in EM2 sleep. There is no need to prevent sleeping for this application. To apply the new configuration on the baud rate, see the section zwave_soc_door_lock_keypad.slcp.

app_cli_cc_user_credential.c#
  • Rename u3c_user struct type to u3c_user_t.

  • Rename u3c_credential struct type to u3c_credential_t.

  • Rename u3c_event_data_validate struct type to u3c_event_data_validate_t.

  • Rename u3c_event_data_learn_read_done to u3c_event_data_learn_read_done_t.

  • Rename u3c_credential_metadata to u3c_credential_metadata_t.

  • Rename u3c_credential_learn_event_data to u3c_event_data_learn_start_t.

  • When calling CC_UserCredential_move_credential_and_report(...), remove slot argument.

  • In function definition u3c_move_credential_slot(...), use CC_UserCredential_move_credential(...) instead of CC_UserCredential_move_credential_and_report(...).

    • According to the specification, this action is no longer supported. The lifeline group cannot be notified about this change.

app_credentials.c#
  • Rename u3c_user struct type to u3c_user_t

  • Rename u3c_credential struct type to u3c_credential_t

  • Rename u3c_credential_learn_event_data to u3c_event_data_learn_start_t

zwave_soc_door_lock_keypad.slcp#
  • Do the steps described in General steps for all applications

  • Additionally, add the following configuration to the .slcp file:

    - name: SL_IOSTREAM_EUSART_VCOM_BAUDRATE
      value: 9600 # In EM2 the eusart is working only with 9600 baud
    - name: SL_IOSTREAM_EUSART_VCOM_ENABLE_HIGH_FREQUENCY # Disable high frequency mode for EUSART to work in EM2
      value: 0
    - name: SL_CLOCK_MANAGER_WDOG0CLK_SOURCE
      value: CMU_WDOG0CLKCTRL_CLKSEL_LFRCO
    - name: SL_CLOCK_MANAGER_EUSART0CLK_SOURCE
      value: CMU_EUSART0CLKCTRL_CLKSEL_LFRCO
    

Led Bulb#

All steps are explained in section General steps for all applications.

Multilevel Sensor#

app.c#
  • Add #include "app_pm_transition_event.h".

  • Add these lines after RadioConfig = zaf_get_radio_config();:

    #ifdef SL_CATALOG_ZW_PM_TRANSITION_EVENT_PRESENT
      // register callback from power manager transitions
      ZW_PmTransitionEventInit();
    #endif
    
app_btn_handler.c#
  • See General steps for all applications

app_sleep_callbacks.c#
  • Add the following include:

    #include "sl_board_control_config.h"
    #if SL_BOARD_ENABLE_SENSOR_RHT || SL_BOARD_ENABLE_SENSOR_IMU
    #include "sl_board_control.h"
    #endif
    
  • Add at the end of void EMU_EM4PresleepHook(void):

    #if SL_BOARD_ENABLE_SENSOR_RHT
      sl_board_disable_sensor(SL_BOARD_SENSOR_RHT);
    #endif
    #if SL_BOARD_ENABLE_SENSOR_IMU
      sl_board_disable_sensor(SL_BOARD_SENSOR_IMU);
    #endif
    
MultilevelSensor_interface_icm20689.c#

See General steps for all applications

MultilevelSensor_interface_nosensor.c#

See General steps for all applications

MultilevelSensor_interface_sensor.c#

See General steps for all applications

Switch On Off#

All steps are explained in section General steps for all applications.

Power Strip#

All steps are explained in section General steps for all applications.

Sensor PIR#

app.c#
  • Add #include "app_pm_transition_event.h".

  • Add these lines after RadioConfig = zaf_get_radio_config();:

    #ifdef SL_CATALOG_ZW_PM_TRANSITION_EVENT_PRESENT
      // register callback from power manager transitions
      ZW_PmTransitionEventInit();
    #endif
    
app_btn_handler.c#
  • See General steps for all applications

app_cli.c#
  • Add #include <string.h> to suppress compiler warning about the implicit declaration of the strcmp function.

SensorPIR_UserTask_DataAcquisition.c#
  • See General steps for all applications

Wall Controller#

All steps are explained in section General steps for all applications.

7.23.0#

How to migrate legacy HMIs to Silicon Labs based solution#

General Information#

In the 7.23 Z-Wave release, Silicon Labs changed the legacy button and LED handling to the Silicon Labs platform provided solution. This document describes how to migrate the legacy human-machine interfaces (from 7.19) to the Silicon Labs based solution. This document can be divided into two parts: one will describe the new components that have been introduced in the 7.23 release; and the other part will describe how to migrate a 7.22 project to the 7.23 release.

New components#

SL Simple Button#

The Simple Button Driver provides an implementation of the Generic Button API. This driver supports both active high and low buttons and configurable debouncing. This component is instantiable, meaning that several named instances can be created. For each instance a configuration is generated along with an initialization struct set according to this configuration. These instance defines and variables are available in a generated header file, sl_simple_button_instances.h. Selecting this component will also include the Simple Button Core component, which is the implementation of the Simple Button driver itself. API Reference

SL Simple LED#

The Simple LED Driver provides an implementation of the Generic LED API. This driver supports controlling GPIO based on/off type LEDs. This component is instantiable, meaning that several named instances can be created. For each instance a configuration is generated along with an initialization struct set according to this configuration. These instance defines and variables are available in a generated header file, sl_simple_led_instances.h. Selecting this component will also include the Simple LED Core component, which is the implementation of the Simple LED driver itself. API Reference (5.0.2)

SL App Button Press#

The Button Press component is used for handling the button state, which can be:

  • Button is not pressed,

  • Button is pressed for a short duration,

  • Button is pressed for a medium duration,

  • Button is pressed for a long duration,

  • Button is pressed for a very long duration and

  • Button has just been pressed down.

This component is built on SL Simple Button. Button press duration for various lengths is configurable and each end user can configure it according to their needs.

Differences in the project structure#

In this document, the most complex project will be used as an example, which is the Z-Wave SoC Door Lock Keypad project. In the following table, the differences in the source files can be seen between the 7.22 and 7.23 projects.

7.22 Top Project Stucture

7.23 Top Project Stucture

app_btn_handler.c

app_cc_battery_callbacks.c

app_cc_door_lock_callbacks.c

app_cc_event_handlers

app_cc_event_handlers

app_cli.c

app_cli.c

app_cli.h

app_cli.h

app_credentials.h

app_credentials.h

app.c

app.c

events.h

events.h

main.c

main.c

The main differences are:

  • app_btn_handler.c (API change)

  • app_cc_battery_callbacks.c

  • app_cc_door_lock_callbacks.c (API change)

Crucially, with this release, application related sources files like platform\SiliconLabs\AppsHw\src\DoorLockKeyPad\DoorLockKeyPad_hw.c were removed. All application related logic was moved to the application project's directory. In this case, DoorLockKeyPad_hw.c was split into three separated sources: app_btn_handler.c, app_cc_battery_callbacks.c and app_cc_door_lock_callbacks.c.

Migrating the app_btn_handler.c file#

In previous releases, button and LED configurations were spread out across multiple files. From the 7.23 release, Silicon labs switched to the standard SiSDK components to handle those peripherals, such as sl_simple_button and sl_simple_led. Because of those components, we can use Simplicity Studio's Pin Tool to remap a button or LED pin in the application. There is no need to do any additional configuration regarding these peripherals.

 

Buttons#

Previously, button handling was implemented in platform\SiliconLabs\AppsHw\src\<application>\<application>_hw.c source files, in this case DoorLockKeyPad_hw.c. Now, this logic can be found in the application's directory, in app_btn_handler.c. A helper SiSDK component, called app_button_press, is also used to generate events on button pressing, such as short, medium or long press events. The duration of these events can be configured in app_button_press_config.h header file, in the config directory inside of the application project's directory. In case you had any custom logic regarding the button handling in platform\SiliconLabs\AppsHw\src\<application>\<application>_hw.c, in this example, DoorLockKeyPad_hw.c, please move them to the app_btn_handler.c file in the application project's directory.

In app_btn_handler.c, only the app_button_press_btn_0_handler or app_button_press_btn_1_handler functions need to be handled, which take the duration as an input parameter. Those callbacks are called automatically when a button event is fired.

 

LEDs#

LED handling was simplified, which means LEDs can be manipulated via sl_simple_led API calls. They can also be configured using the Pin Tool. No additional configuration is required. In case you are using functions prefixed with Board_ to manipulate LEDs or GPIOs, please use the sl_simple_led and em_gpio components' API from 7.23 release.

Migrating the app_cc_<command class>_callbacks.c files#

There are new source files in every application, named in the pattern app_cc_<command class name>_callback.c. In the new structure, each of those sources contain callbacks for a specific command class. These callbacks can be different in every application, e.g. battery report callback, which can be different in a real life application compared to a sample application. From the 7.23 release, such callbacks are exposed on the application level. In this example, battery command class related callbacks are in the application project's directory, named app_cc_battery_callback.c. If you had any custom implementation of command class specific callbacks in platform\SiliconLabs\AppsHw\src\<application>\<application>_hw.c files, in this case DoorLockKeyPad_hw.c, please move those implementations next to the application, into the related source file.