The Credential descriptor table is an array of associations between unique Credentials and file IDs of Credential metadata objects.

A Credential is identified by its owner's User Unique ID and the Credential's type and slot. Only the entries from ZAF_FILE_ID_CC_USER_CREDENTIAL_USER_BASE to ZAF_FILE_ID_CC_USER_CREDENTIAL_USER_BASE + n_credentials - 1 are to be considered valid.

Public Attribute Documentation#

user_unique_identifier#

uint16_t credential_descriptor_t_::user_unique_identifier

credential_slot#

uint16_t credential_descriptor_t_::credential_slot

object_offset#

uint16_t credential_descriptor_t_::object_offset

credential_type#

u3c_credential_type credential_descriptor_t_::credential_type