structure used to describe the format of a get region info answer.

Public Attributes#

uint8_t
uint8_t

the region supports classic Z-Wave

uint8_t

the region supports Z-Wave Long Range

uint8_t

reserved for future use

uint8_t

the selected region include this one (e.g. US_LR include US)

Public Attribute Documentation#

region#

uint8_t serial_api_setup_cmd_get_region_info_answer_t::region

zw_classic#

uint8_t serial_api_setup_cmd_get_region_info_answer_t::zw_classic

the region supports classic Z-Wave


zw_lr#

uint8_t serial_api_setup_cmd_get_region_info_answer_t::zw_lr

the region supports Z-Wave Long Range


reserved#

uint8_t serial_api_setup_cmd_get_region_info_answer_t::reserved

reserved for future use


included_region#

uint8_t serial_api_setup_cmd_get_region_info_answer_t::included_region

the selected region include this one (e.g. US_LR include US)