Bring-Up/Test HW Development User's Guide#
NOTE: This section replaces UG523: Bring-Up/Test HW Development User's Guide. Further updates to this user guide will be provided here.
This document describes how to use the RAILTest software to perform RF bring-up tests and validate a design based on the following Z-Wave 700 and 800 devices:
ZGM130S and EFR32ZG14 (700 series)
ZGM230S and EFR32ZG23 (800 series)
Key Points#
Provides hardware design considerations for bring-up and validation
Gives guidelines how to test RF performance of a Z-Wave product
Provides a basic guide of RAILtest to measure Z-Wave devices
Audience and Prerequisites#
The audience for this document is Z-Wave hardware developers and test engineers working with the development, bring-up test, and validation test of Z-Wave hardware using Z-Wave 700 and 800 devices. It is assumed that the reader has a basic knowledge of RF metrics and Z-Wave as such.
The prerequisites are:
Access to Simplicity Studio
A PC with a UART terminal program
A Z-Wave development kit or hardware containing a Z-Wave 700 or 800 device with UART access
Access to RF measurement equipment, such as an RF Spectrum Analyzer and an RF generator