Deprecated List#
Global CC_UserCredential_send_association_report (u3c_credential_metadata_t const *const p_source_metadata, u3c_credential_metadata_t const *const p_destination_metadata, u3c_user_credential_association_report_status_t const status, RECEIVE_OPTIONS_TYPE_EX *const p_rx_options)
Global E_SYSTEM_TYPE
Use Application Node Info instead
Global FUNC_ID_APPLICATION_SLAVE_COMMAND_HANDLER
OBSOLETE: In DevKit 4.5x/6.0x Controller Bridge applications, this is obsoleted by the FUNC_ID_APPLICATION_COMMAND_HANDLER_BRIDGE
Global FUNC_ID_GET_TX_COUNTER
Global FUNC_ID_ZW_SET_EXT_INT_LEVEL
Global Transport_ApplicationCommandHandlerEx (RECEIVE_OPTIONS_TYPE_EX *rxOpt, ZW_APPLICATION_TX_BUFFER *pCmd, uint8_t cmdLength)
If all command classes use one of the REGISTER_CC macros, this function is not required to be implemented in the application. There exists a weak definition of it. ZAF_CC_Invoker will take care of invoking the right command class handler.
Global Transport_OnLearnCompleted (node_id_t nodeID)
Global zpal_tx_power_t
Global ZW_TX_POWER_10DBM
Global ZW_TX_POWER_14DBM
Global ZW_TX_POWER_20DBM